Video of the Week – How the CRM rotary module can guide cable lengths of up to 4.5m
21/05/2020

20th May, 2020
The CRM rotary module is part of the e-spool flex range and can guide any type of cable or hose, and even corrugated tubes.
This compact module has a maximum rotation angle of 6480°, which is 18 full turns, for cable lengths up to 4.5m with a maximum speed of 180°/s and acceleration of 180°/s².
As it does not use a slip ring, it is very easy to use, more flexible, less susceptible to faults and splash waterproof. Each component of the CRM can be replaced separately, including the cable or hose.
Compared to the TB12 twisterband, the CRM rotary module requires a lower clearance height for the same maximum rotation angle (6480°). The rotary module’s clearance height is less than 10cm, while the twisterband is more than 25mm.
Areas of application include material handling, machine tools, industrial robots, medical technology, telescopes and antennas.
To watch the video showing the CRM in action, please visit: www.igus.co.uk/rotarymoduleVOTW or https://youtu.be/IETFeI4nYO4
For more information about the CRM rotary module, please visit: www.igus.co.uk/info/rotary-module or call igus directly on: 01604 677240.
The terms igus, Apiro, chainflex, CFRIP, conprotect, CTD, drylin, dry-tech, dryspin, easy chain, e-chain, e-chain systems, e-ketten, e-kettensysteme, e-skin, flizz, ibow, igear, iglidur, igubal, kineKIT, manus, motion plastics, pikchain, plastics for longer life, readychain, readycable, ReBeL, speedigus, triflex, robolink, and xiros are protected by trademark laws in the Federal Republic of Germany and internationally, where applicable. All other registered trademarks and trademarks are the property of their respective owners.