The switch to igutex® polymer bearings for long standing customer and agricultural equipment manufacturer Sumo UK Ltd, has allowed them to produce longer lasting, durable machinery and save on the cost of standard metal bearings that require lubrication. Finding bearings that are cost-effective, tough enough to take on the most heavy-duty loads, and that minimise […]
Through downsizing, the draw-e-chain saves 30% in costs in applications with occasional movement igus has launched the draw-e-chain for cable routing in drawers and pull-out applications like server racks. Thanks to its minimal structural design, this compact energy chain costs 30% less than that of the most cost-effective standard e-chains. This prevents costly oversizing, especially […]
The first batch of the famous all-plastic igus bicycle is in production, while igus builds a high-volume production line. The day has finally come. After months of development, the igus:bike, a bicycle made of 92% plastic with a high proportion of recycled material, is in production. The first 100 bikes are being produced while igus […]