Customised, modular machine building with Module Connect at Zemat
29/07/2024

Module Connect helps machine builder Zemat to produce customised “plug & play” modules for their Boxmat HD cardboard packaging machine, allowing the quick and smooth coupling of table modules for different sized boxes.
In the super-competitive machine building industry, companies are looking for a manufacturing advantage so machines can be assembled more quickly and easily. Zemat Technology Group, a leading manufacturer of packaging machinery, has designed a modular system using the igus® Module Connect system to help their customers add modular stations to upgrade base machines quickly.
Module Connect from igus® is a modular plug-in connector for connecting several services in one coupling, such as electric cables, fibre optic and encoder cables, and pneumatic hoses. The space-saving industrial connector is designed for plug-and-play use. Zemat designs and manufactures a range of machines such as sealing machines, cutting plotters, and industrial automation production lines. One of their biggest product lines is a cardboard packaging machine. The Boxmat HD is the most advanced and versatile in the range, allowing the customer to make short and medium production runs of different corrugated boxes by changing the table module.
A Boxmat HD customer needed a system for easy coupling and decoupling of additional modules – a feeder table. The solution needed to integrate control, communication, pneumatic, and sensor cables in a single multi-connector, that was able to mechanically connect connectors to sockets, in a modular design, allowing one of three variants to be connected to each base machine. It should be small and allow for future expansion.
Perfect outcome with Module Connect and Harting Han inserts
Zemat designed, manufactured, and commissioned a bespoke solution that met all customer requirements, that combines Harting Han inserts with the igus Module Connect. Zemat worked together with igus® to develop the optimal interface: three Module Connect modules permanently mounted to the machine housing. igus® selected suitable control cables (CF130.05.12.UL, CF130.05.18.UL series), communication cables in CAT5e standard (CFBUS.PVC.045 series) and pneumatic cables (CAPU.A.06.0 series) and delivered the whole system as a prefabricated cable harness.
Zemat also developed a system for precisely guiding the machine’s modules so that the electrical connectors are not damaged during assembly.
The entire Module Connect system can be expanded with additional machine modules, allowing customisation of future machine versions – for example, adding an additional printer behind the feed table.
Zemat customer Klaus Rumpp was pleased with the modular solution. “Zemat supplies intelligent, reliable machines. Communication is pleasant and staff can answer all questions quickly. The goal is not short-term sales, but rather long-term customer loyalty for mutual benefit. Their obligations for this project have been fulfilled without exception. Thank you Zemat, for your support and we look forward to further cooperation.”
“Module Connect was developed from direct customer feedback, that customers wanted a single, plug-and-play master connector for all services from energy to data and fibre optics, that docks to the machine with ease” says igus® UK managing director Matthew Aldridge. “It’s great to see that Zemat has built a perfect working example of this. We are developing similar solutions for customers in the UK – please get in touch for more details.”
Zemat is the first serial machine manufacturer in Poland to build a range of industrial machines with the Module Connect; the winner of the Red Dot Design Award in 2018.
For more information about this case study visit:
(Please note this page is only available in Polish)
https://www.igus.pl/info/module-connect-on-the-boxmat-machine-zemat-packaging-industry
https://www.igus.co.uk/info/module-connect-for-furniture-production
For more information on this product, please contact:
Erin Kemal
Tel: 01604 677240
Email: ekemal@igus.co.uk
Taylor Macdonald
Tel: 01604 677240
Email: tmacdonald@igus.net