First recyclable plastic bicycle frame made by igus®
05/08/2024

motion plastics specialist igus supplies the first injection-moulded bike frame made of composite material for e-bike manufacturer Advanced Bikes
First, igus® launched the RCYL Bike, a bicycle made from recycled fishing nets. Now the company is setting the next milestone for sustainable mobility: a company first, it has developed an injection moulded bicycle frame made of recyclable composite material for the e-bike manufacturer Advanced Bikes. Knowledge acquired over decades in plastics processing and the experience gained with the RCYL bike helped develop both the frame and new components made of high-performance plastics.
It is predicted that in 2024, e-bikes will be the most popular type of bicycle purchased in the UK[i]. This trend is partly driven by environmental concerns, as 90% of today’s bicycle frames are made of aluminium or carbon, produced in energy-intensive processes and end up in huge bicycle landfills at the end of their life.
To help drive the transformation to a circular economy, e-bike manufacturer Advanced Bikes is relying on igus® for their future frame production. The companies have worked together to develop a sustainable, composite material bicycle frame for use in the new Reco Urban trekking e-bike. “Advanced’s aim was to produce a frame from a composite material with 100% recyclable plastic using injection moulding,” says Matthew Aldridge, managing director at igus® UK. “Since we have been developing components such as plain bearings, rod ends, and gears for the bicycle industry for over 30 years, we immediately took on the challenge of supporting Advanced in the bicycle frame design and taking over development, tooling and injection moulding.”
New frame protects the environment
To ensure that the frame has sufficient strength, stiffness and low weight, igus® uses a composite material in granulate form, consisting of high-performance plastics and carbon fibres. It also designed and made a multi-part injection moulding tool for the complex geometry of the bicycle frame within a few weeks. The result: a 3.3kg lightweight bicycle frame injected moulded in a single part – no welds, corrosion-resistant, durable and tested.. igus® is also able to regranulate end-of-life frames via its own “chainge” recycling programme, recycling the material. “In the future, we want to have other recyclable bicycle components such as luggage racks, rims, spokes and seat posts, all manufactured using injection moulding,” explains Helge von Fugler, founder and managing director of Advanced. “This is the only way to make a completely recyclable e-bike a reality.”
Lubrication-free, high-performance plastic components
igus® currently produces bicycle frames using two different processes In injection moulding, both components and frames are produced in one piece. Frames are also manufactured using rotationa moulding, such as for the RCYL bike. But it’s not just about bicycle frames. igus® has huge knowledge in plastics processing and this product development experience are now being used for new bicycle components – from wheels to cranks, from handlebars to planetary gears. Large and small volume production can therefore be carried out cost-effectively. In addition, these high-performance plastic components are lighter, lubrication-free and corrosion-free. Users can reach for the high-pressure cleaner because no lubricant is washed out and nothing can rust.
Maximum safety due to numerous test attempts
igus® tests all components extensively before use. 135 trillion test cycles and 15,000 trials take place every year in their test laboratory, 250m2 of which are used to test bicycle components, including the new Reco frame. “We will test the first injection-moulded bike frames with computed tomography for problems such as air pockets in the composite material and carry out all relevant frame tests in our laboratory,” says Aldridge. Customers receive a 30-year warranty from Advanced Bikes. For maximum safety, igus® uses a variety of test methods. “These are based on standard tests, for example by the EFBE (specialist bicycle standards agency) and the TÜV,” says Aldridge. igus® also conducts its own test procedures, including the use of a climate chamber, the data from which can be used to make precise statements about the service life of igus materials under different environmental conditions.
Everything from one source: from design to finished product
“With bicycle components made of high-performance plastic, we offer the bicycle industry access to a completely new technology,” says Aldridge. “In this way, we also offer solutions to OEM manufacturers who want to implement their own ideas and designs with us.” By using plastic, developers can completely rethink bike design and geometry. And at igus®, they receive everything from a single source: from design to research and development, toolmaking, compounding, testing and production to recycling. Just-in-time production means that igus® can deliver quickly, and stock capacities at the customer’s premises can be reduced. The business is more predictable and profitable due to “make to order”.
The Advanced Bikes Reco Urban trekking e-bike with single moulded plastic frame can be seen at https://advancedbikes.uk/reco-2024/.
For more information on this product, please contact:
Taylor Macdonald
Tel: 01604 677240
Email: tmacdonald@igus.net
[i] Is the bike industry in recovery? UK bike sales expected to reach £1 billion in 2024 with ebikes leading the charge | BikeRadar).