New particle-free energy chain from igus for SCARA robots in cleanrooms

Published on: 21/09/2023

Clean SCARA Cable Solution works almost particle-free to ISO class 2 igus has launched a new energy supply system for SCARA robots in cleanrooms: the Clean SCARA Cable Solution consists of tribologically optimized high-performance plastics and works in almost particle-free conditions specified to ISO class 2 even in high-speed applications. The system is also highly […]

Read more...

igus tests plastic bearings on wooden shafts, finds friction values comparable to some metals

Published on: 20/09/2023

A new design study by igus demonstrates how smooth linear plain bearings made of recycled material work when fitted on wooden shafts. Drylin Econ-G bearing J4 proves to be a winner with wood. Is wood and plastic a good combination in engineering? Motion plastics specialist igus has investigated this question in a new design study, […]

Read more...

Swimming pool on demand

Published on: 06/09/2023

A Conmag Engineering solution can transform a terrace into a pool while saving EU30,000 with the help of corrosion-free linear technology from igus Conmag Engineering has designed a “mobile pelvic floor” that transforms a luxury swimming pool into a walk-on terrace using linear technology engineering from igus that works reliably and with little maintenance under […]

Read more...

Cheers! igus linear guide taps beer in seconds

Published on: 30/08/2023

Food engineering company One Two Beer GmbH develops automatic beer dispensing system with igus drylin linear technology for foam-free pouring. To prevent long queues at busy bars, One Two Beer GmbH has developed an automatic beer dispensing system. The centre piece is a mobile dispensing head that inserts into the bottom of cups and enables […]

Read more...

From 6 weeks to 7 days. New igus system makes custom moulded bearings super-fast

Published on: 17/08/2023

FastLine service with online configurator from igus for developers in the any industry Automotive designers and buyers are accustomed to long lead times. To make an injection moulding tool for a mass-produced, wear-resistant special component, they would typically have to wait up to six weeks. Time that igus can now reduce to just seven days […]

Read more...