Pick and place applications are becoming increasingly popular within companies wanting to automate processes. These can be simple movements to complex actions but fundamentally the movements all need the same thing… to be smooth running. In this weeks’ video of the week, you can see how igus® products ranging from energy chains to linear gantries […]
“Tech up, cost down” is proudly on display at MACH 2022 as motion plastics specialist igus exhibits a new low-cost robot for small scale work and a novel solution for storing and shipping cable drums – both increasing efficiency but keeping costs down. Automating industrial and lab-based operations is becoming more popular with labour shortages […]
In the UK we have over 200KM of chainflex® cable so can keep your machines moving! In this week’s video of the week, you get a sneak preview into why we are number one! Our continuous testing, our 36-month guarantee and being UL verified all ensure we can provide the best to our customers. To […]
The plug-in principle of readychain micro-speed enables fast connection of e-chain systems in small installation spaces igus has launched a plug-and-play energy chain system called readychain speed that allows connection of fully assembled e-chain systems in seconds, with no tools needed. This reduces assembly throughput times or machine downtime, and planned maintenance work can be […]
Have you ever considered the movement of a turnstile or an automated gate? Nowadays the advancement in the technologies used at these gates, such as facial recognition and body scanners, it is more than just an open and shut movement. In this week’s video of the week, adjustable facial recognition screens are shown using various […]
Lubrication- and maintenance-free xiros stainless steel support roller ensures safe operation thanks to electrostatic dissipation. Sparks caused by a lack of electrostatic dissipation can lead to expensive failures of machines and systems, and in the worst case can lead to explosions. To increase protection, igus has introduced a dissipated version of its lubrication- and maintenance-free […]
In this week’s video of the week, the packaging machine showcases a number of igus® products being used. From curved rail to drylin® and iglidur® bearings, all products are ideally suited for this application as no maintenance is required. The igus® products are also lubrication free so allows a clean, smooth motion. The machine also […]
Pick and place and simple assembly operations in medical labs and electronics production lines can now be engineered at low cost, with the latest robot from igus, the drylin SCARA. One common barrier to automating a manufacturing process, certainly in the UK, has been cost. Motion plastic and cable technology pioneers igus devised the Low […]
In this week’s video of the week, the ease in which a cable can be inserted into one of our energy chains is clear. Whether it is air, liquid or hydraulics being carried within the chain, the cables are protected and can be changed quickly if required. To view the video, click here https://youtu.be/TUgHgXzwN2I For […]
Long service life of igus chainflex high-end TPE cables convinces inspectors and gives customers certified safety igus is the first cable manufacturer in the world to receive UL AWM certification from US validation agency Underwriters Laboratories (UL) for its high-end TPE cables, which do not require fire-retardant halogens as additives. This is the first time […]