chainflex
25th November, 2019 igus is pleased to announce the official opening of its automated assembly line for readycable at its UK facility in Northampton. Representing another significant investment for company, the new line uses fully-automated machines and lean manufacturing methods to streamline its manufacturing process to deliver fully-harnessed drive cables shipped within 24 hours of […]
17th November, 2019 The use of automated guided vehicles (AGVs) in factories and warehouses is booming. They work around the clock, 7 days a week, 365 days a year. For AGV manufacturers, achieving maximum uptime is a challenge, which can be overcome by using reliable and maintenance-free components. “iglidur tribopolymer bearings, which are used in […]
12th November, 2019 igus has introduced the e-loop energy chain for safe cable management on top drives for deep drilling rigs. The new modular system, which is made of high-performance plastic, ensures a defined minimum bend radius of the cables and withstands adverse weather conditions, as well as vibration and shock. In addition to use […]
3rd October, 2019 Guiding power, data and media in confined spaces at high speeds is a major challenge for many OEMs, in particular for intralogistics. With the micro flizz, igus offers a compact energy guidance system for travels up to 100 metres. It consists of an energy chain, flexible chainflex cables suitable for tight bend […]
24th September, 2019 igus has developed its first plastic-steel hybrid energy chain for telescopic applications, such as cherry pickers, telehandlers and boom lifts. Compared to conventional steel energy chains which are sometimes used in these applications, the new YE.42 e-chain is half the weight. It also provides up to 10m unsupported travel, which is 50% […]
September 3rd, 2019 With the e-skin flat and the e-skin soft, igus offers two new space-saving energy chain systems for use in cleanroom applications. Developed for tight installation spaces on short, self-supporting travels, e-skin soft is made of a softer material than the standard e-skin. As the name suggests, e-skin flat is for very flat […]
27th March, 2020 A team of undergraduates at Surrey University are pioneering Formula Student in the UK with an all-electric powertrain. Formula Student is the world’s largest student motorsport competition, which brings together teams from universities across the world. Team SURTES (Surrey University Racing Technology Engineering Solutions) operates out of the Engineering Design Centre in […]