dry-tech
The new generation of the strain wave gear is low cost, self-lubricating and polymer! With high efficiency, no lubrication and its lightweight design, the dry running strain wave gear is a welcomed addition to the drygear® family. In this week’s video of the week, you can see how easy it to assemble and how the […]
Lubrication-free and maintenance-free high-load material iglidur TX2 demonstrates 3.5-fold improved wear performance in tests. Especially forhigh-load applications in the construction, machinery, or agricultural industries, igus can now offer the new Tribo (tribologically optimized) material iglidur TX2, which works without lubrication. Even smaller excavating machines still need about 50 litres of lubricant per year with metal […]
iglidur rollers with predictable service life ensure product transport in food technology So that users can get their wear-resistant knife edge roller even faster, igus has expanded its online shop to include the range of iglidur rollers made from high-performance polymers. Included in the new range are knife edge rollers made of the blue material […]
Electrostatically dissipating iglidur AX500 tribopolymer ensures maintenance-free, food industry applications In the food and packaging industry, sorting and packing zones are subject to constant movement of goods and temperature changes. For these storage mechanisms to perform flawlessly, long-lasting plain bearing solutions are required that can withstand friction and heat long-term. Another challenge is the creation of […]
2021 seems to be the year of the drone. In this week’s video you will be introduced to the “drone in the box” system. This allows drones to fly autonomously and automatically, it also serves as a landing platform, control box and offers a station for recharging the battery. In the video, you can see […]
The manus award- igus’s awards programme for polymer bearing applications, received 582 entries in 2021. Back in 2019, The iFLY15 catamaran won silver in the manus awards and is now attempting to break a world record. Twin-hulled catamarans are designed to lift out of the water on hydrofoils, and the iFLY15 sports catamaran from CEC […]
Tribo-polymers showcase their advantages in maintenance-free and lubrication-free iglidur bearing technology Assessing the service life of a machine must take account of the costs of purchase, procurement and installation, as well as all the costs incurred in the long term operation, maintenance and repair of the machine. Using wear-resistant materials and low-maintenance components reduces not […]
FDA-compliant polymer coating powder with four times longer service life than IC-01 boosts wear-resistance Sheet metal and metallic parts in food processing are regularly exposed to friction and wear. Motion plastics experts igus has developed a new coating material to increase the service life of these components, by reducing friction and wear. The IC-05 tribo-polymer […]
January 2021: A category to reward sustainability has been added to this year’s Manus Awards – an event organised by igus to celebrate manufacturers using engineering plastics and bearing systems in their designs. 2021 is the tenth anniversary of its prestigious Manus Awards and to mark the occasion igus has added a Green category to […]
Rollers made of a new iglidur A250 high-performance polymer, enable faster conveyor belt speeds Motion plastics expert igus have designed and manufactured a new high-performance polymer ideally suited for the growing demands of the food production sector. The new iglidur A250 tribo-polymer, designed and manufactured by igus, whose UK headquarters are in Northampton, is the […]