dry-tech
24th October, 2019 The Falkland Islands are an archipelago comprising two main islands and 778 smaller islands covering an area of 12,000 sq km (almost half the size of Wales) with a population of just over 3.5 thousand. Here, a radio station covers local news and the territory’s only newspaper is Penguin News. The islands […]
24th October, 2019 For lubrication-free sliding in a very tight space, igus has introduced a new coating material and service for metal components. The iglidur coating provides the components with the wear and sliding properties of the maintenance-free iglidur materials. The coating was developed for applications where a classic shaft-bearing combination is not possible, such […]