Category:

e-chain

Robot takes over the grape harvest

Published on: 18/12/2024

Cheers! Wine harvester designs autonomous “steep slope” harvesting vehicle with igus energy chains Christmas means friends, food and, for many, a few drinks. White wine is the most popular alcoholic beverage in the UK1 and we consume about £12bn of alcohol in the four weeks leading up to Christmas2. To keep supplying wine, especially with […]

Read more...

Clear your desk: the igus OfficeChain cuts desk clutter for more efficient working 

Published on: 21/10/2024

Ergonomic innovations meet elegant design to improve office desks   The popularity of height-adjustable desks for ergonomic working is growing fast. Cable routing inside the desk is essential to avoid cable clutter, snag and tripping hazards. Now igus has the perfect solution – the OfficeChain OCO.32.37.0. Due to the easy handling and simple design, this […]

Read more...

The perfect loop for offshore operations 

Published on: 19/08/2024

The innovative igus e-loop can now easily allow a single damaged cable to be changed in the top drive of a jack-up rig in offshore oil & gas operations.  When a cable is damaged in the top drive system of a jack-up rig, normally the entire “service loop” with all cables and hoses must be […]

Read more...

Smooth entertainment aboard, even in rough seas thanks to igus and Videlio-HMS

Published on: 17/06/2024

At French shipyard Chantiers de l’Atlantique, theatres and entertainment systems supplied by Videlio-HMS must pass rigorous standards to run smoothly at sea. Cables and energy supply systems supplied by igus are chosen for their reliability and maritime standards. Life at sea is very different to life on dry land; ask any seafarer. And all the […]

Read more...

New igus compact low-cost energy chain designed for drawers

Published on: 02/05/2024

Through downsizing, the draw-e-chain saves 30% in costs in applications with occasional movement igus has launched the draw-e-chain for cable routing in drawers and pull-out  applications like server racks. Thanks to its minimal structural design, this compact energy chain costs 30% less than that of the most cost-effective standard e-chains. This prevents costly oversizing, especially […]

Read more...

snapchain 2.0: Compact, low carbon, and cost-effective energy management

Published on: 14/11/2023

New igus energy chain can be installed in seconds and is the second igus e-chain series to be made of 100% recycled material. The simplest products are often both the most cost-effective, and the best technically. igus has now developed snapchain 2.0, a sustainable energy chain especially for simple, flat cable packages made of 100% […]

Read more...

Wanted: Unique applications for energy chain systems, igus vector awards

Published on: 31/10/2023

Win up to 5,000 euros as the ninth “vector award” for different and sustainable e-chain solutions opens for applications. Deadline: February 9, 2024 Attention all machinery engineers: The vector award from igus has entered the next round. For the ninth time, the award recognises designers and project managers who show creativity and imagination in the […]

Read more...

Highest safety in battery production: first energy chain to be certified for dry cleanrooms

Published on: 01/08/2023

Test passes with flying colours: igus’ E6.29 energy chain receives innovative dry cleanroom certificate from research consultancy Fraunhofer IPA for ISO Class 4 Whenever the highest hygiene standards are required, igus scores well with lubrication-free and abrasion-resistant motion plastic components. A topical example is that battery production for electric vehicles requires special environmental conditions, which are […]

Read more...

VOTW- How to make applications in Material handling work more efficiently

Published on: 22/06/2023

There are so many applications within the material handling industry that need reliable, effective, and durable products, so it is hardly surprising that there are so many igus® products used in these applications. In this week’s “video of the week”, we see a small selection of igus® parts in action in material handling, from drylin® […]

Read more...

Microphone reeler primed to be smash hit with stage and theatre engineers at ABTT 2023

Published on: 05/06/2023

Stage and concert performers struggling with microphone stands can put this in the past as a clever Microphone Motor Reeler from igus solves a common snag in the stage technology industry. Plus igus will show its e-spool flex and zigzag products at the ABTT 2023 show. When the lead singer takes the stage at Reading, […]

Read more...