Category:

e-chain

VOTW- e-chains® at work in various automotive applications

Published on: 20/04/2023

With the automotive industry being such a high cost per hour, it is vital that all machinery runs as smoothly as possible and with minimal maintenance. In this weeks, “video of the week”, you can see a variety of applications within the automotive industry that use igus® energy chains. From the robotic triflex® series to […]

Read more...

Better cable stowage for EV charge points

Published on: 22/11/2022

igus presents a design study for a compact, automatic cable management system for electric vehicle chargers A quick pull and the power cable retracts: With the new automatic cable management system called e-tract 2.0, igus wants to make charging electric vehicles at charge points more convenient for EV owners. And thanks to a sophisticated interplay […]

Read more...

VOTW-Cost-effective, lighter and sustainable. Why more Automotive engineers are turning to plastic.

Published on: 03/11/2022

In this current financial struggle, it is no wonder why the automotive industry has been looking at alternatives for expensive, heavy and environmentally damaging components. In this week’s video of the week, the humble car seat is cast into the spotlight, highlighting the various areas of the seat that can be fitted with igus® lubrication-free […]

Read more...

STS container cranes: new heavy-duty roller chain from igus helps future-proof tomorrow’s ports

Published on: 01/11/2022

The P4HD.56.R energy chain designed for container cranes is built for long travel distances, high speeds, heavy cable fills and Industry 4.0 connectivity to prevent costly failures Container cranes in busy commercial ports will be even faster and more powerful in the future. In response igus has launched P4HD.56. R – a new heavy-duty energy […]

Read more...

Save water in farming with roller e-chain for targeted irrigation

Published on: 18/10/2022

A new precision irrigation carriage can reduce water and fertiliser consumption by up to 75%, and an igus e-chain in a trough guides hoses with an additional energy saving. The aim of the precision irrigation carriage made by Rathmakers Gartenbautechnik is to use the right amount of water while also conserving groundwater resources. The new […]

Read more...

World’s first driven e-chain system for very long travels, by igus

Published on: 04/10/2022

igus’s new, drive-chain has high dynamics, integral load support, long service life and can save up to six tons of weight for port cranes. Commercial port operations use rail-bound Automated Stacking Cranes (ASC) to process high volumes of shipping containers. These, and other applications that require long e-chain travels, will benefit from a new drive-chain […]

Read more...

VOTW- Want to go racing? Greaves 3D and igus® bring racing to students at Northampton university

Published on: 30/09/2022

igus®, Greaves 3D Engineering and the University of Northampton came together to introduce the new racing simulator. This has been developed by Greaves 3D Engineering and features approx 45 igus® components from; bearings, linear rails, drives to various types of e-chains®. These racing simulators are being used as part of the esports BSc degree course […]

Read more...

GO! Greaves 3D and igus take the lead in race to perfectly simulate motorsport

Published on: 15/09/2022

A super-realistic racing simulator has been developed by Greaves 3D Engineering that features 45 igus bearings, linear rails, drives and e-chains. The University of Northampton is using the simulator for deployment on its esports BSc degree course. The driver grips the contoured steering wheel lightly and adjusts the seat position forward, angled back. The pedal […]

Read more...

World’s first e-chain made of 100% recycled material: igus drives circular economy forward  

Published on: 16/08/2022

Conserving resources and extending the product life cycle are the objectives of the new igus cradle-chain E2.1.CG, which saves 28% CO2 versus current e-chain production.  From cradle to cradle: The goal of the circular economy is to return consumables to the biological or technical cycle in order to conserve valuable resources and raw materials, retain […]

Read more...

Use, recycle, reuse: igus makes e-chain recycling even easier

Published on: 12/07/2022

igus installs and now also removes old energy chains for customers Since 2019 igus has given old energy chains a second life by recycling them under the “chainge” recycling program. Now the motion plastics specialist is going one step further. Because an upgrade often means installing a whole new system, igus removes old energy chains […]

Read more...