Category:

e-chain

Compact and bijou: The e-spool flex mini guides cables safely and saves space

Published on: 26/01/2022

Compact, desktop energy supply system from igus transmits power, data and media without interruption, and without a slip ring It is 169mm high, 163mm long, 78mm deep and weighs only 200 grammes, making the e-spool flex mini from igus one of the smallest and lightest cable and hose reels in the world. It carries energy, […]

Read more...

No dramas: Reliable energy supply for various stage technology demands with igus e-chains and e-spools

Published on: 18/01/2022

Complicated stage applications can be implemented even in confined spaces and with high loads using moving energy supply systems such as the e-spool and the zig-zag systems. The challenge for every stage and set builder is to design and build the perfect stage. Every job is different because stages are not off-the-shelf. Every stage is […]

Read more...

IPA test passed! e-skin flat energy chain with three layers receives cleanroom Class 1

Published on: 30/11/2021

The award-winning, modular alternative to ribbon cable proves its particle-free qualities in Fraunhofer cleanroom test. In clean room environments such as laboratories, energy chains required to manage cables and hoses safely must be particle-free. igus has developed the e-skin flat, an economical alternative to ribbon cables due to its modular design. Proof that the energy […]

Read more...

Vector highlights: Showcasing the best of the 2020 nominees.

Published on: 19/11/2021

It is that time again for the vector awards! Showcasing the best of energy chain applications. There are always innovative applications, and this year will be no exception. Thanks to Covid, last year’s vectors were postponed so the 2022 ones will be bigger and better! In this week’s video of the week, we look back […]

Read more...

VOTW- E4.1 and one for all

Published on: 28/10/2021

This versatile energy chain demonstrates its unique features in this video of the week. These features make it suitable for almost any cable management application, offering high strength, low wear, low noise, and a host of other design details that make it easy and fast to use.  The possibilities for this energy chain are endless.   Click here to view the video https://youtu.be/D3feMi2sEvY For more information […]

Read more...

Wanted: novel energy supply applications for biennial €5k prize and award

Published on: 26/10/2021

The vector award for unique energy chain applications is entering its eighth round. Applications are open now, with deadline for entries 11 February 2022. Rotating 7,000 degrees, travelling at speeds of 10 m/s and moving in multiple dimensions: they are energy chains made from high-performance plastics. Every two years, an expert panel awards the best […]

Read more...

VOTW-e-chains® on the side

Published on: 09/09/2021

Whether it be vertical or horizontal the igus® e-chain® will protect your cables. In this week’s video of the week, you can see how the igus® e-chains® are used on their side. No restrictions to the movement, no interruption to power, no problem. Click here to view the video https://youtu.be/BM7p-QdUSmU For more information on igus® […]

Read more...

Sustainability at the push of a button: e-chain for Drop Water vending machine

Published on: 07/09/2021

A new water vending machine from a Californian company reduces the transport and consumption of plastic bottles with the help of igus motion plastics. The Drop Station is a new sustainable drinks vending machine that dispenses water into compostable containers at the push of a button. The water does not have to be transported, as […]

Read more...

Cost down, life up with Vertical farming

Published on: 26/08/2021

This week’s video shows how igus products are used in vertical farming, an exciting new industry which demands reliability, longevity and no maintenance.  This is perfect for igus motion plastics, from smooth gliding drylin® gantries to robust, lightweight e-chains®, the elimination of lubrication means no contamination. To view the video, click here https://youtu.be/lFbmUTzMPXk For more […]

Read more...

VOTW- igus® motion plastics for drone equipment

Published on: 20/08/2021

2021 seems to be the year of the drone. In this week’s video you will be introduced to the “drone in the box” system. This allows drones to fly autonomously and automatically, it also serves as a landing platform, control box and offers a station for recharging the battery.  In the video, you can see […]

Read more...