Plain bearing
Lubrication-free igus plain bearings allow new, go-anywhere electric stand-up vehicle to operate in even the most difficult environmental conditions An electric version of man’s most dependable and versatile friend, the horse, is now a reality. Canadian company LyteHorse Labs has designed a novel all-terrain electric vehicle, suitable for many applications and environmental conditions. igus bearings […]
Have you ever considered all the applications where things turn? There are thousands!! And to help these applications turn with a smooth motion, customers are using the igus® PRT slewing ring bearing. These bearings are low-cost, maintenance free and require no lubrication! In this weeks’ video of the week, the PRT shows the ease to […]
Sometimes having a nonstandard part can be problematic and expensive. Thankfully with the igus® stock material range, this doesn’t need to be the case. With a large variety of materials, with different temperature ranges and different mechanical properties, the iglidur® stock materials are suitable for a multitude of applications. In this week’s video of the […]
In this week’s video of the week, Head of the iglidur® gears business unit Steffan Shchack introduces injection moulded polymer gears from igus® From stock, we have 3 designs in a variety of wear resistant materials, suitable for applications with high temperatures, electrically conductive and high endurance. From one gear to a million, we can […]
Lubrication-free and maintenance-free high-load material iglidur TX2 demonstrates 3.5-fold improved wear performance in tests. Especially forhigh-load applications in the construction, machinery, or agricultural industries, igus can now offer the new Tribo (tribologically optimized) material iglidur TX2, which works without lubrication. Even smaller excavating machines still need about 50 litres of lubricant per year with metal […]
iglidur rollers with predictable service life ensure product transport in food technology So that users can get their wear-resistant knife edge roller even faster, igus has expanded its online shop to include the range of iglidur rollers made from high-performance polymers. Included in the new range are knife edge rollers made of the blue material […]
Electrostatically dissipating iglidur AX500 tribopolymer ensures maintenance-free, food industry applications In the food and packaging industry, sorting and packing zones are subject to constant movement of goods and temperature changes. For these storage mechanisms to perform flawlessly, long-lasting plain bearing solutions are required that can withstand friction and heat long-term. Another challenge is the creation of […]
2021 seems to be the year of the drone. In this week’s video you will be introduced to the “drone in the box” system. This allows drones to fly autonomously and automatically, it also serves as a landing platform, control box and offers a station for recharging the battery. In the video, you can see […]
Two new lubrication-free tribo polymers increase the service life of bearings in single-axis solar trackers Solarmid and iglidur P UV are the names of the two new materials that igus has developed specifically for housing bearings in single-axis solar trackers, the panels that track sunlight in solar farms. The new polymers last much longer than […]
igus now offers injection moulded, cost-effective production of lubrication-free gears Gears made of polymer deliver power transmission in many applications, from automatic coffee machines to actuators. Specifically for producing wear-resistant and durable gears, igus now offers injection moulded gears in addition to machining from bar stock and those made using additive manufacturing (3D printing). Customers […]