Keyword:

automotive industry

VOTW- e-chains® at work in various automotive applications

Published on: 20/04/2023

With the automotive industry being such a high cost per hour, it is vital that all machinery runs as smoothly as possible and with minimal maintenance. In this weeks, “video of the week”, you can see a variety of applications within the automotive industry that use igus® energy chains. From the robotic triflex® series to […]

Read more...

VOTW- xiros® ball bearings in several applications

Published on: 24/11/2022

xiros® plastic ball bearings are light-weight, corrosion and chemical resistant and require no lubrication. These qualities enable them to be acquired in a vast variety of applications across many industries. In this week’s video of the week, we illustrate our plastic ball bearings in a selection of application examples, from the automotive industry to conveyor […]

Read more...

VOTW- How can a ball bearing work in the automotive industry?

Published on: 25/08/2022

This is quite a common question and in this week’s video of the week, the question is answered. The xiros® range of polymer ball bearings are low friction, cost-effective and dirt resistant. Not only that, but they are also quiet which is crucial in Automation. So, in answer to the question, ball bearings are perfect […]

Read more...

New igus elastic double joint proves a quiet solution for labelling machines

Published on: 23/02/2021

A new elastic double joint from plastics specialist igus is proving to be a perfect – and quiet – solution for the machine building sector. The igubal GPZM coupling joint, which was officially launched at the end of 2020, is lubrication-free, maintenance-free and 20% more flexible than its conventional alternative. Dean Aylott, Product Manager at […]

Read more...