ball bearing
xirodur MT180 meets the world’s strictest safety standards and reduces certification costs of medical technology products Motion plastics specialist igus is expanding its range of high-performance plastics for medical technology. New in the medical range is xirodur MT180, a material for lightweight, lubrication-free, and hygienic xiros deep groove ball bearings – certified to the strictest […]
This is quite a common question and in this week’s video of the week, the question is answered. The xiros® range of polymer ball bearings are low friction, cost-effective and dirt resistant. Not only that, but they are also quiet which is crucial in Automation. So, in answer to the question, ball bearings are perfect […]
The combination of great design and clever, novel materials produces a resilient and quiet tribo-optimized ball bearing for high speed and low noise. Following intense research and development, igus has launched a novel two-component (2K) ball bearing. The lubrication- and maintenance-free xiros bearing combines several properties making it wear-resistant and dimensionally stable and quiet, even […]