bearings
January 2021: A category to reward sustainability has been added to this year’s Manus Awards – an event organised by igus to celebrate manufacturers using engineering plastics and bearing systems in their designs. 2021 is the tenth anniversary of its prestigious Manus Awards and to mark the occasion igus has added a Green category to […]
New felt seals have been designed and manufactured by igus to protect iglidur plain bearings from the adverse effects when running in excessive amounts of sand, dirt, and abrasive dust. The global manufacturer of energy chain systems and polymer plain bearings,which has its UK headquarters in Northampton, has developed this additional method of protection specifically […]
Lubrication-free tribo-polymers ensure the reliable operation of vertical farming systems. Motion plastics from igus are playing a major role in the increasingly popular sector of vertical farming. igus, which has its UK headquarters in Northampton, is working closely with global companies specialising in vertical farming – the practice of growing plants indoors in stacked layers […]
31st July, 2020 igus® offers a large range of lubrication-free polymer bearings which can cope with high loads, high speeds and high temperatures. With attributes such as these, it is no wonder that they are ideal for utilising within motorcycles. These maintenance-free parts deliver a long service life and can, in some cases, improve performances […]
31st March, 2020 Linear systems are extensively used to move doors, monitors or even panels laterally, or side-to-side. If a low driving force is required, especially for manual adjustments, rollers are often used in the bearing element to reduce friction. However, to absorb the lateral forces, the position of these rollers is crucial. As a […]