cables
Automating production is becoming the focus of many companies and Axis Harvesting is no exception. From weighing to packaging the punnets, automation helps alongside humans to process over 90 tonnes of mushrooms per week. In this week’s video you can easily spot the bright blue igus® Th3 hygienic energy chain, cable managing the igus® readycables! […]
Sea locks commonly use festoon systems and with that can come issues with maintenance. This is why customers are changing from festoon systems to igus® energy chains. In this week’s video of the week, the igus® e-chain® is shown powering the sea lock with ease. After retrofitting in 2006, replacing a festoon system, a further […]
Renowned globally for engineering innovation, igus is set to exceed expectations with a head-turning, maintenance-free product that will really shake up the way we travel. The future of transportation is here! It is true, this claim has been made many times before, but innovation leaders igus believe they have created a real breakthrough in low-cost […]
New flexible chainflex cable saves 40% space ine-chains and ensures secure energy and data transmission The next generation of motors are designed to be small, compact, and fast, and more and more drive manufacturers are relying on hybrid technology to save space. In response, igus has now expanded its range of hybrid cables with a […]
New small rotary module for robots, handling and camera systems saves up to 73% cost It’s lightweight, compact and made entirely of plastic: the new Polymer Rotation Module (or PRM) rotary energy supply system from igus. igus has now developed a system comprising a polymer energy chain and a low-friction plastic guide channel especially for […]
The igus e-loop, a heavy duty energy chain for drilling machinery, has won an international award recognising its design to protect cables/hoses and operators on oil & gas platforms. igus has returned a winner at the prestigious International Association of Drilling Contractors (IADC) NSC Safety Awards in Aberdeen for the innovative e-loop, a clever product […]
In the UK we have over 200KM of chainflex® cable so can keep your machines moving! In this week’s video of the week, you get a sneak preview into why we are number one! Our continuous testing, our 36-month guarantee and being UL verified all ensure we can provide the best to our customers. To […]
Long service life of igus chainflex high-end TPE cables convinces inspectors and gives customers certified safety igus is the first cable manufacturer in the world to receive UL AWM certification from US validation agency Underwriters Laboratories (UL) for its high-end TPE cables, which do not require fire-retardant halogens as additives. This is the first time […]
igus has introduced ready-made cables for the Single Pair Ethernetespecially for e-chain use Single Pair Ethernet (SPE), which uses a single twisted pair of conductors that reduces the cable thickness and the size of the connectors required, is now one of the biggest trends in data communication for devices to communicate with the smallest sensors. […]
Compact, desktop energy supply system from igus transmits power, data and media without interruption, and without a slip ring It is 169mm high, 163mm long, 78mm deep and weighs only 200 grammes, making the e-spool flex mini from igus one of the smallest and lightest cable and hose reels in the world. It carries energy, […]