cables
15th April, 2020 The challenge for every stage engineer is to create the perfect set, while meeting all related safety and building code standards. In this week’s video, igus shows a range of technologies developed specifically for theatre and stage construction. Here, there are technically challenging requirements, which include high loads, such as those found […]
12th April, 2020 Simple, precise, fast processes: these are the requirements of Cartesian robots. They are used for such things as pick & place applications, sorting systems and medical technology. igus has now developed a line and room linear robot for large workspaces. The two new kinematics systems allow users to move up to 5kg. […]
25th November, 2019 igus is pleased to announce the official opening of its automated assembly line for readycable at its UK facility in Northampton. Representing another significant investment for company, the new line uses fully-automated machines and lean manufacturing methods to streamline its manufacturing process to deliver fully-harnessed drive cables shipped within 24 hours of […]
17th November, 2019 The use of automated guided vehicles (AGVs) in factories and warehouses is booming. They work around the clock, 7 days a week, 365 days a year. For AGV manufacturers, achieving maximum uptime is a challenge, which can be overcome by using reliable and maintenance-free components. “iglidur tribopolymer bearings, which are used in […]
September 3rd, 2019 With the e-skin flat and the e-skin soft, igus offers two new space-saving energy chain systems for use in cleanroom applications. Developed for tight installation spaces on short, self-supporting travels, e-skin soft is made of a softer material than the standard e-skin. As the name suggests, e-skin flat is for very flat […]
27th March, 2020 A team of undergraduates at Surrey University are pioneering Formula Student in the UK with an all-electric powertrain. Formula Student is the world’s largest student motorsport competition, which brings together teams from universities across the world. Team SURTES (Surrey University Racing Technology Engineering Solutions) operates out of the Engineering Design Centre in […]