corrosion resistant
The first batch of the famous all-plastic igus bicycle is in production, while igus builds a high-volume production line. The day has finally come. After months of development, the igus:bike, a bicycle made of 92% plastic with a high proportion of recycled material, is in production. The first 100 bikes are being produced while igus […]
Simply switching to a polymer bearing from a stainless-steel bearing has saved a lead acid battery recycler, Fry’s Metals thousands in maintenance costs, and far more in preventing lost production time Recycling lead batteries in high volume is a tough, corrosive working environment to work in. As such, one of South Africa’s leading lead recycling […]
High load capacity, and smooth operation: xiros plastic ball bearings from igus make a big difference in a range of applications in overhead conveyor technology. As digital transformation increases manufacturing throughput, and with booming online trade, the demands on material handling are constantly increasing. Customers expect faster and more reliable deliveries, meaning order structures and […]