Keyword:

drylin linear technology

Two drives in one: igus launches dual drive stepper motor

Published on: 06/02/2024

New stepper motor for drylin linear axes provides space-saving and cost-effective dual drive To help customers get started with automation, especially where space is limited, igus has developed a new dual drive stepper motor for its drylin linear technology. It can be used to drive two linear systems directly, which also saves space. Another potential […]

Read more...

Swimming pool on demand

Published on: 06/09/2023

A Conmag Engineering solution can transform a terrace into a pool while saving EU30,000 with the help of corrosion-free linear technology from igus Conmag Engineering has designed a “mobile pelvic floor” that transforms a luxury swimming pool into a walk-on terrace using linear technology engineering from igus that works reliably and with little maintenance under […]

Read more...

Cheers! igus linear guide taps beer in seconds

Published on: 30/08/2023

Food engineering company One Two Beer GmbH develops automatic beer dispensing system with igus drylin linear technology for foam-free pouring. To prevent long queues at busy bars, One Two Beer GmbH has developed an automatic beer dispensing system. The centre piece is a mobile dispensing head that inserts into the bottom of cups and enables […]

Read more...