dryspin
Food engineering company One Two Beer GmbH develops automatic beer dispensing system with igus drylin linear technology for foam-free pouring. To prevent long queues at busy bars, One Two Beer GmbH has developed an automatic beer dispensing system. The centre piece is a mobile dispensing head that inserts into the bottom of cups and enables […]
Harmonised lead screws and lubrication-free lead screw nuts in trapezoidal threads extend service life by 30%. Motion plastics specialist igus has refined the classic trapezoidal thread, achieving a 30% service life extension – a huge increase for a well-established mechanical part. Thanks to a special geometric interaction between the lead screw nut, which requires no […]
2021 seems to be the year of the drone. In this week’s video you will be introduced to the “drone in the box” system. This allows drones to fly autonomously and automatically, it also serves as a landing platform, control box and offers a station for recharging the battery. In the video, you can see […]
19th May, 2020 In its virtual trade show, igus presents more than 100 plastic innovations and product range additions from all areas of motion plastics. Around 400 square metres in size, the real stand is now open to online visitors and follows the theme ‘Cost down, Life up. It’s our job’. The trade show is […]