e-chain
Renowned globally for engineering innovation, igus is set to exceed expectations with a head-turning, maintenance-free product that will really shake up the way we travel. The future of transportation is here! It is true, this claim has been made many times before, but innovation leaders igus believe they have created a real breakthrough in low-cost […]
New flexible chainflex cable saves 40% space ine-chains and ensures secure energy and data transmission The next generation of motors are designed to be small, compact, and fast, and more and more drive manufacturers are relying on hybrid technology to save space. In response, igus has now expanded its range of hybrid cables with a […]
It is vital to keep offices and personal workspaces clear from loose cables. Not only is this important for aesthetics but also from a safety point of view, loose cables can be hazardous. In this weeks’ video of the week, you can see that with its modular design, the office chain is easily lengthened and […]
New small rotary module for robots, handling and camera systems saves up to 73% cost It’s lightweight, compact and made entirely of plastic: the new Polymer Rotation Module (or PRM) rotary energy supply system from igus. igus has now developed a system comprising a polymer energy chain and a low-friction plastic guide channel especially for […]
The igus e-loop, a heavy duty energy chain for drilling machinery, has won an international award recognising its design to protect cables/hoses and operators on oil & gas platforms. igus has returned a winner at the prestigious International Association of Drilling Contractors (IADC) NSC Safety Awards in Aberdeen for the innovative e-loop, a clever product […]
igus has introduced ready-made cables for the Single Pair Ethernetespecially for e-chain use Single Pair Ethernet (SPE), which uses a single twisted pair of conductors that reduces the cable thickness and the size of the connectors required, is now one of the biggest trends in data communication for devices to communicate with the smallest sensors. […]
Moving cable applications with different orientations can cause designers issues. How can you get moving power vertically/horizontally/rotationally? With the range of energy chain variations available with igus®, there is a solution for your application. In this week’s video of the week, you can see the different vertical options for long horizontal travels. Options ensuring power […]
Complicated stage applications can be implemented even in confined spaces and with high loads using moving energy supply systems such as the e-spool and the zig-zag systems. The challenge for every stage and set builder is to design and build the perfect stage. Every job is different because stages are not off-the-shelf. Every stage is […]
The award-winning, modular alternative to ribbon cable proves its particle-free qualities in Fraunhofer cleanroom test. In clean room environments such as laboratories, energy chains required to manage cables and hoses safely must be particle-free. igus has developed the e-skin flat, an economical alternative to ribbon cables due to its modular design. Proof that the energy […]
In this video you can see the comparison between the assembly time of an igus® plastic cobot clamp and the metal version. There simply is no comparison when it comes to the speed, however the metal ones can sometimes be the better option when there is a faster motion. Luckily igus® offers both options! So, […]