iglidur
Founded in Ireland, Ecovolve is transforming the construction industry with innovative electric and eco-friendly machinery. The company’s journey, rooted in ambition and ingenuity, has since grown into a pioneering force in sustainable construction equipment. Ecovolve’s inception dates back to 2008, a challenging year marked by the onset of the global recession. Founder, Sean Breen, previously […]
The plastics industry is preparing for a potential ban of fluoropolymers, or PFAS, a group of versatile polymers that have many industrial applications. igus® has increased R&D resources for developing viable non-PFAS solutions, and is working with customers in automotive, medical, packaging and other industries, to find fully tested alternative materials if required. Motion plastics […]
igus launches a new lubrication-free material, for bearings needing higher running performance with high dynamic forces, ideal for heavy-duty applications. igus has developed plain bearings made from high-strength, fibre-wound materials – the igutex bearing family. These use carbon fibre embedded in the material and are used where very high impact loads occur and where injection-moulded […]
New generation of igubal spherical plain bearings are equipped with a predictive maintenance system Costly machine failures due to undetected defects in demanding applications should soon be made redundant, thanks to a new generation of two- and four-hole flange bearings with “smart” features. The lubrication-free high-performance plastic bearings are equipped with miniature wireless sensors that […]
Metal bearings are still popular for designers, but plastic bearings are replacing traditional metallic solutions more and more, either in new designs or to replace those old broken, rusting or wearing bearings. But are plastic bearings up to the challenge of withstanding the same forces, temperature and environmental pressures of metallic ones? In this “video […]
As well as increasing the number of low carbon and renewable products and services in 2023, igus uses a reliable carbon tracking method for suppliers and can now provide the carbon content of most iglidur products. It aims to show the carbon content of all its products by mid-2024. Companies are under growing pressure to […]
The igus ReBeL cobot now has a humanoid hand made of lubrication-free, high-performance plastics Robots are increasingly finding their way into small and medium-sized companies, especially as collaborative robots or “cobots”, such as the igus ReBeL. These robots sort, pick and move items with the help of cameras and mechanical or vacuum gripping systems. To […]
iglidur Q3E plain bearings, now manufactured by injection moulding, ensure lubrication-free maximum load capacity performance, made using efficient high-volume production An important industry first for the construction and agricultural machinery industries: For the first time igus has found a way to manufacture heavy-duty bearings made from two components of high-performance plastic, using the cost-effective injection […]
Simply switching to a polymer bearing from a stainless-steel bearing has saved a lead acid battery recycler, Fry’s Metals thousands in maintenance costs, and far more in preventing lost production time Recycling lead batteries in high volume is a tough, corrosive working environment to work in. As such, one of South Africa’s leading lead recycling […]
Thanks to ultra-delicate teeth, new wear-resistant micro gears are suitable for particularly precise applications Whether in micro-drives, microscopes or precision engineering, engineers are building ever more compact products. Motion plastics specialist igus now produces micro gears with a module – the unit of gear tooth size – of up to 0.2. Thanks to high-performance plastics, […]