Keyword:

iglidur

New polymer spherical ball from igus improves food safety and lowers cost

Published on: 30/08/2022

The new material iglidur A181 makes the igubal food contact joint system three-times more wear ­resistant and has several food safety features. To make machines and systems for the food industry even safer, igus has launched the high-performance plastic iglidur A181, a new standard for a spherical ball material for the igubal food contact (FC) […]

Read more...

Listen carefully: igus develops innovative two-component, very quiet ball bearing

Published on: 09/08/2022

The combination of great design and clever, novel materials produces a resilient and quiet tribo-optimized ball bearing for high speed and low noise. Following intense research and development, igus has launched a novel two-component (2K) ball bearing. The lubrication- and maintenance-free xiros bearing combines several properties making it wear-resistant and dimensionally stable and quiet, even […]

Read more...

Metal out, plastic in: igus presents new lubrication-free plain bearings for heavy industry

Published on: 20/07/2022

Bearing points on construction and agricultural machinery can be free of lubrication and maintenance with iglidur M210 and M260 materials Save time and costs on bearings for machinery medium loads with iglidur M210 and M260. These materials enable heavy machinery like construction equipment to switch from thick-walled metal bearings to plastic bearings with no structural […]

Read more...

VOTW-Plain bearings in the construction industry

Published on: 14/07/2022

The construction industry requires robust, durable and reliable products to be used within the machinery. In this week’s video of the week, igus® products are shown in various aspects of construction machinery, showing that plastic bearings are more than capable of withstanding the construction life! Being lubrication free, igus® products are ideal for use in […]

Read more...

Lubrication-free, plastic-metal rod ends: for better hygiene and higher loads in the food sector

Published on: 21/04/2022

igubal stainless steel rod ends with iglidur A160 enable lubrication-free dry running with no risk of contamination Constant relubrication of metal bearing points in the food industry costs time, money and increases the risk of contamination. Maintenance-free igubal spherical plain bearings from igus are an economical and safe alternative. Now igus has introduced a new […]

Read more...

VOTW- Motion plastics in automatic gates

Published on: 21/03/2022

Have you ever considered the movement of a turnstile or an automated gate? Nowadays the advancement in the technologies used at these gates, such as facial recognition and body scanners, it is more than just an open and shut movement. In this week’s video of the week, adjustable facial recognition screens are shown using various […]

Read more...

VOTW- igus® products in packaging machines.

Published on: 11/03/2022

In this week’s video of the week, the packaging machine showcases a number of igus® products being used. From curved rail to drylin® and iglidur® bearings, all products are ideally suited for this application as no maintenance is required. The igus® products are also lubrication free so allows a clean, smooth motion. The machine also […]

Read more...

When speed counts: FastLine delivers injection-moulded special plain bearings in 7 days

Published on: 22/02/2022

New toolmaking production line enables rapid delivery of customised igus plain bearings Industrial parts and products must be delivered quickly and reliably, but the manufacture of special parts by injection moulding can take several weeks. Plastics specialist igus has expanded its in-house toolmaking department and can now offer its customers the “FastLine” express service. Lubrication-free, […]

Read more...

VOTW- 3D Printing goes large!

Published on: 20/01/2022

You can now print big! Really big! Up to 3M with igus®! With the iglidur® large format printing capabilities, 3D printed parts of up to 3M are now not a problem. With a variety of materials, including FDA materials, the possibilities are endless. In this week’s short video of the week, you can see large […]

Read more...

Horse 2.0: Electric LyteHorse can conquer city, farm, forest and desert

Published on: 07/12/2021

Lubrication-free igus plain bearings allow new, go-anywhere electric stand-up vehicle to operate in even the most difficult environmental conditions An electric version of man’s most dependable and versatile friend, the horse, is now a reality. Canadian company LyteHorse Labs has designed a novel all-terrain electric vehicle, suitable for many applications and environmental conditions. igus bearings […]

Read more...