Industry 4.0
“ReBeLs on Wheels” make driverless transport systems affordable through modern plastic technology. Mobile robotics systems are being used in more and more industries, in e-commerce warehouses as well as modern restaurants. Conventional models on the market start at around 25,000 euros, while solutions with an integrated robot arm start at around 70,000 euros. However, widespread […]
A new igus communication module combines i.Sense sensors and the “superwise” service for low-cost, fast and reliable condition monitoring in real time to avoid costly failures. Optimising operational processes and minimising downtime: the iComm Box from igus can help. Inside the new communication module, igus i.Sense condition monitoring sensors are smoothly integrated into “superwise” – […]
But that’s not all: igus constantly develops its smart plastics services to respond to challenges such as the shortage of skilled workers. For example, thanks to an igus digital service called “superwise“, it is easier now ever to monitor all one’s applications via a central dashboard with less expenditure on personnel. This connection, by the […]
New generation of igubal spherical plain bearings are equipped with a predictive maintenance system Costly machine failures due to undetected defects in demanding applications should soon be made redundant, thanks to a new generation of two- and four-hole flange bearings with “smart” features. The lubrication-free high-performance plastic bearings are equipped with miniature wireless sensors that […]
Make your energy chain system intelligent. Adding a sensor unit to your machine helps prevent breakdowns, can save you time and money and keep your production line running. The i.Sense EC.W system allows a direct connection from the energy chain system to the control, offers real-time monitoring of the e-chain wear and ensures continuous supply. […]
The world’s first plastic gearbox for cobots and access to a digital ecosystem: latest igus Low Cost Automation product records 20 new projects per week in Germany alone Low cost and about 8kg, the plug-and-play ReBeL cobot is one of the lightest cobots on the market. Digital services provided with it, such as the RBTXpert and […]
igus develops P4HD roller e-chain with wear-resistant materials, and smart monitoring. Next generation cranes need higher power supplies. Energy chains – the protective chains that transport power and control cables in linear motion – must meet these requirements for longer travels, higher accelerations and operational uncertainties, as well as high reliability. The new igus heavy-duty […]
New i.Cee:local module predicts the service life of machines and manufacturing systems, making maintenance more efficient and predictable Motion plastics leader igus has developed a new predictive maintenance device, a new home for the software to power its smart plastics products – the i.Cee:local module. The module calculates the remaining service life of the energy […]
Industrial robots are pervasive in manufacturing and their applications are increasing all the time. But with constant multi-axis movements, the cables that supply robots are subjected to extreme levels of stress, posing a challenge for manufacturers of cables and other connecting components. The International Federation of Robotics predicts that by 2020 more than 1.7 million […]
Printed components made intelligent – this is the latest product development from motion plastics experts igus. In this world first, igus can integrated sensors into its printed motion plastics components to predict maintenance requirements and avoid downtime. igus, which has its UK headquarters in Northampton, has developed a special feature; sensors are directly printed into […]