Keyword:

linear

Safety at high speed with the igus e-chain system in a linear motor robot

Published on: 12/08/2020

12th August, 2020 Side-mounted energy chain from igus ensures reliable energy supply in high-speed lightweight linear robots Twice as fast at half the weight: this is what makes the linear motor robot from FIBRO LÄPPLE TECHNOLOGY (FLT) different from many other solutions. In order for the linear robot to be able to get production up […]

Read more...

A winning combination: the new linear and pivoting slide from igus

Published on: 29/07/2020

29th July, 2020 A drylin W linear guide fitted with a PRT slewing ring bearing provides linear and rotating motion. This new design study from igus can move linearly and rotate simultaneously. With the drylin W linear/pivot guide, armrests, trays and control panels on seats and armchairs, for example, can be easily adjusted to suit […]

Read more...

Fast entry into low-cost automation using a digital twin in intuitive robot control

Published on: 30/06/2020

30th June, 2020 igus has developed control software for its low-cost automation solutions that allows users to easily program their robots. Available online, free of charge, the igus robot control software enables different robot kinematics to be programmed and controlled. A digital twin simulates the movements, allowing the user to program a suitable solution before […]

Read more...

Video of the Week – How igus drylin linear robot technology can help you carry on camping

Published on: 26/06/2020

26th June, 2020 The innovative Camping Butler cleans mobile toilet cartridges, from caravans and camper vans, fully automatically and contact-free from the inside and outside. No matter how full or very dirty the cassette is, the Camping Butler cleans it completely. In the week’s video, we go behind the scenes to see how exactly the […]

Read more...

Video of the Week – How automation is made easy with the modular Apiro system

Published on: 04/06/2020

4th June, 2020 The new modular Apiro motion system from igus, enables design engineers to develop low-cost automation systems with endless possibilities. Consisting three lubrication-free worm gears for standard, inverted and linear movements, which can be connected in series or parallel and configured to perform simple linear motion to complex robotic tasks. The worm gears […]

Read more...

igus supports student spice vending machine project with drylin W linear systems

Published on: 11/05/2020

8th May, 2020 Curry instead of cola! Five students from Heubach, Germany have developed a vending machine for packaged spices together with engineers and trainees from EMAG LaserTec GmbH. To ensure that the salt, curry and pepper cans are picked from their compartments quickly, they used the drylin W linear guides from igus. Putting academic […]

Read more...

Bigger, stronger, faster: new igus drylin linear robots for cost-effective automation

Published on: 15/04/2020

12th April, 2020 Simple, precise, fast processes: these are the requirements of Cartesian robots. They are used for such things as pick & place applications, sorting systems and medical technology. igus has now developed a line and room linear robot for large workspaces. The two new kinematics systems allow users to move up to 5kg. […]

Read more...

igus introduces two new hybrid roller bearings for easy adjustment in lateral positioning systems

Published on: 15/04/2020

31st March, 2020 Linear systems are extensively used to move doors, monitors or even panels laterally, or side-to-side. If a low driving force is required, especially for manual adjustments, rollers are often used in the bearing element to reduce friction. However, to absorb the lateral forces, the position of these rollers is crucial. As a […]

Read more...