Keyword:

lubrication free

VOTW- TX2, Heavy duty for agriculture

Published on: 20/10/2022

Our TX bearings are not injection moulded like our other iglidur® plain bearings. These bearings have an interwoven design, each layer incorporating solid lubricants, which not only means no lubrication but it also increases the mechanical strength compared to moulded bearings. These are ideal for high mechanical loads and are 3 times stronger than their […]

Read more...

VOTW-Plain bearings in the construction industry

Published on: 14/07/2022

The construction industry requires robust, durable and reliable products to be used within the machinery. In this week’s video of the week, igus® products are shown in various aspects of construction machinery, showing that plastic bearings are more than capable of withstanding the construction life! Being lubrication free, igus® products are ideal for use in […]

Read more...

World first at Engineering Expo: igus unveils the world’s first urban bike made from recycled plastic

Published on: 31/05/2022

***VISIT IGUS’s STAND AT ENGINEERING EXPO 8th to 9th JUNE for the UK LAUNCH of the ALL NEW, ALL-PLASTIC igus BIKE*** igus will launch the world’s first all-plastic urban bicycle for the UK market at Engineering Expo on 8th June. Its debut showing was at Hannover Messe on 30th May. Using the igus expertise in […]

Read more...

VOTW- drylin® T: Interchangeable with recirculating ball bearing guides!

Published on: 19/05/2022

Being able to interchange between different suppliers can be priceless when looking for replacements. The drylin® T range is an exact replacement for other linear guides, same dimensions, same hole positions but the drylin® T slides instead of rolls. Not only that, they are 100% lubrication free. To view the similarities as well as the […]

Read more...