Keyword:

lubrication-free

igusGO: AI-driven, cost-saving machine design optimisation app makes work fun

Published on: 07/11/2023

By harnessing AI, a new igus app shows how to optimise the design of over 450 applications in just a few seconds Wouldn’t it be nice if time-poor engineers, faced with huge component choices, could easily and quickly improve their designs by seeing the full range of components and their properties instantly? Step forward the […]

Read more...

Wanted: Unique applications for energy chain systems, igus vector awards

Published on: 31/10/2023

Win up to 5,000 euros as the ninth “vector award” for different and sustainable e-chain solutions opens for applications. Deadline: February 9, 2024 Attention all machinery engineers: The vector award from igus has entered the next round. For the ninth time, the award recognises designers and project managers who show creativity and imagination in the […]

Read more...

The new igus recycled bearing is unveiled

Published on: 17/10/2023

The iglidur ECO series is expanded to include a chemical-resistant ECO P210 variant igus knows that plastic is a valuable resource and waste must be minimised, so it has launched a regranulated compound for the iglidur ECO plain bearing series from sprues and missing parts from injection moulding production. Launched in October 2023, the new […]

Read more...

Calculate the service life of 3D printing materials online in 30 seconds

Published on: 11/10/2023

igus has expanded its 3D printing range for wear-resistant, lubrication-free special parts – now providing service life, costs, material properties and delivery times. Knowing the durability of a 3D-printed component often makes it easier to choose the right material. That’s why igus has added a new service to its 3D printing range. The online service […]

Read more...

Minimal and green: a recycled slewing ring bearing from igus for only £55

Published on: 28/09/2023

igus’ new ready-to-install, low-cost PRT slewing ring bearing, PRT-05-15-PC, is made of regranulated high-performance plastics Affordable, compact, lightweight, and ready to install with just one click: igus’s slewing ring bearings in the iglidur PRT series now have a minimal, low-cost variant. PRT-05-15-PC is both low on price and good for the environment, being made of […]

Read more...

New particle-free energy chain from igus for SCARA robots in cleanrooms

Published on: 21/09/2023

Clean SCARA Cable Solution works almost particle-free to ISO class 2 igus has launched a new energy supply system for SCARA robots in cleanrooms: the Clean SCARA Cable Solution consists of tribologically optimized high-performance plastics and works in almost particle-free conditions specified to ISO class 2 even in high-speed applications. The system is also highly […]

Read more...

igus tests plastic bearings on wooden shafts, finds friction values comparable to some metals

Published on: 20/09/2023

A new design study by igus demonstrates how smooth linear plain bearings made of recycled material work when fitted on wooden shafts. Drylin Econ-G bearing J4 proves to be a winner with wood. Is wood and plastic a good combination in engineering? Motion plastics specialist igus has investigated this question in a new design study, […]

Read more...

Swimming pool on demand

Published on: 06/09/2023

A Conmag Engineering solution can transform a terrace into a pool while saving EU30,000 with the help of corrosion-free linear technology from igus Conmag Engineering has designed a “mobile pelvic floor” that transforms a luxury swimming pool into a walk-on terrace using linear technology engineering from igus that works reliably and with little maintenance under […]

Read more...

Cheers! igus linear guide taps beer in seconds

Published on: 30/08/2023

Food engineering company One Two Beer GmbH develops automatic beer dispensing system with igus drylin linear technology for foam-free pouring. To prevent long queues at busy bars, One Two Beer GmbH has developed an automatic beer dispensing system. The centre piece is a mobile dispensing head that inserts into the bottom of cups and enables […]

Read more...

From 6 weeks to 7 days. New igus system makes custom moulded bearings super-fast

Published on: 17/08/2023

FastLine service with online configurator from igus for developers in the any industry Automotive designers and buyers are accustomed to long lead times. To make an injection moulding tool for a mass-produced, wear-resistant special component, they would typically have to wait up to six weeks. Time that igus can now reduce to just seven days […]

Read more...