rails
Telescopic slides are used within all kinds of applications, from kitchens, furniture to aircraft and automotive. This new NTP-27 all polymer telescopic slide is manufactured using igus®‘ iglidur® materials giving all the benefits of our dry running maintenance free and lubrication free dynamics whilst having the added aesthetic feature of many different colour options to […]
29th July, 2020 A drylin W linear guide fitted with a PRT slewing ring bearing provides linear and rotating motion. This new design study from igus can move linearly and rotate simultaneously. With the drylin W linear/pivot guide, armrests, trays and control panels on seats and armchairs, for example, can be easily adjusted to suit […]
31st March, 2020 Linear systems are extensively used to move doors, monitors or even panels laterally, or side-to-side. If a low driving force is required, especially for manual adjustments, rollers are often used in the bearing element to reduce friction. However, to absorb the lateral forces, the position of these rollers is crucial. As a […]