roller e-chain
A new precision irrigation carriage can reduce water and fertiliser consumption by up to 75%, and an igus e-chain in a trough guides hoses with an additional energy saving. The aim of the precision irrigation carriage made by Rathmakers Gartenbautechnik is to use the right amount of water while also conserving groundwater resources. The new […]
igus develops P4HD roller e-chain with wear-resistant materials, and smart monitoring. Next generation cranes need higher power supplies. Energy chains – the protective chains that transport power and control cables in linear motion – must meet these requirements for longer travels, higher accelerations and operational uncertainties, as well as high reliability. The new igus heavy-duty […]