An England-based piano builder is striking a new chord in the design of the centuries-old musical instrument by incorporating tribopolymer components from igus in a unique hammer system that offers supreme longevity, climate resistance and improved playability and sound performance.
Ball tables are used if delicate or heavy goods are to be transported in different directions. The ball transfer units from igus are manufactured with the high performance plastic xirodur B180, which absorbs loads of up to 500 N. igus, which is based in Germany, runs its North American operations out of Providence, R.I.
High speeds on long travels are special challenges for energy chain systems on machines and plants. Therefore, igus has now developed a new glide bar made of high-performance plastics with a five times longer service life. To monitor the wear-resistant rail, users now have the smart plastics EC.T sensor. This provides regular information about the condition of the rail and sends important technical information to the maintenance engineer in good time.