29th April, 2020 Every day, sensors generate vast amounts of data worldwide and this continues to rise. Single Pair Ethernet (SPE) technology offers completely new opportunities to transmit these data streams reliably even in the most confined areas of the machine. Developed for use in energy chains, igus introduces the chainflex CFBUS.PUR.042 SPE cable. While […]
24th April, 2020 The e-skin energy chain system provides cleanroom equipment with data, power and media without unwanted particles contaminating the air, as proven by the Fraunhofer Institute IPA. All three e-skin energy chain types, with and without cables, have ISO Class 1 certification, which is the ‘cleanest’ classification. In the test conducted by the […]
Whether in handling applications or in laboratory equipment, where there is movement, energy chains are widely used to protect and guide cables and hoses. In the medical industry, however, higher demands are placed on the components, which must all run very smoothly and quietly, be cleanroom-compatible, media-resistant and corrosion-free and of hygienic design. In this […]
15th April, 2020 The challenge for every stage engineer is to create the perfect set, while meeting all related safety and building code standards. In this week’s video, igus shows a range of technologies developed specifically for theatre and stage construction. Here, there are technically challenging requirements, which include high loads, such as those found […]
12th April, 2020 Simple, precise, fast processes: these are the requirements of Cartesian robots. They are used for such things as pick & place applications, sorting systems and medical technology. igus has now developed a line and room linear robot for large workspaces. The two new kinematics systems allow users to move up to 5kg. […]
7th April, 2020 igus has now added two new sizes to its twisterband HD range with inner heights of 11mm and 18mm. The key advantage over slip ring systems is that it guides electrical, fibre optic and pneumatic cables all together. Target applications include rotary tables and robots. twisterband HD energy chains are already being […]
31st March, 2020 Linear systems are extensively used to move doors, monitors or even panels laterally, or side-to-side. If a low driving force is required, especially for manual adjustments, rollers are often used in the bearing element to reduce friction. However, to absorb the lateral forces, the position of these rollers is crucial. As a […]
17th March, 2020 igus has developed an intelligent bearing that warns of specific wear level, enabling machine and equipment operators to plan maintenance, repairs or part replacement in advance. Called smart iglidur, the intelligent plain bearing was developed for difficult-to-access bearing points and for applications where no regular maintenance intervals have been planned. Defects are […]
10th March, 2020 Robust, lightweight and maintenance-free; these are the key features of the high-performance e-chains from igus. To ensure reliability for users, igus now offers a 36-month guarantee on its e-chains, which matches the similar chainflex cable guarantee. With the online service life calculator, users can now determine the guaranteed runtime of their e-chain […]
25th February, 2020 High speeds on long travels are distinct challenges for energy chain systems. To overcome these issues, igus has developed a more wear resistant glide bar, which has a service life that is five times longer. Integrated into the rail is the smart plastics EC.T sensor monitors the condition of the rail and […]