Hard on the outside, smart on the inside: igus develops intelligent plain bearing
15/04/2020

17th March, 2020
igus has developed an intelligent bearing that warns of specific wear level, enabling machine and equipment operators to plan maintenance, repairs or part replacement in advance. Called smart iglidur, the intelligent plain bearing was developed for difficult-to-access bearing points and for applications where no regular maintenance intervals have been planned.
Defects are detected before they occur, downtimes are avoided, repair times are shortened due to early intervention, and machine availability is increased. Scheduled maintenance inspections, therefore, become unnecessary.
The body of the new smart iglidur plain bearing consists of two components: the internal, lubrication-free iglidur material and an outer support polymer shell for protection. To measure the amount of wear, an intelligent sensor is mounted between the two components.
The measured data of the sensor can be used in various ways. For example, it is possible to inform the operator about the plain bearing’s wear with a warning light. For high-end applications, the data can be sent directly to a control system, which, after analysis, passes the data on to a customised web interface via the icom communication module for the purposes of maintenance and repair.
For more information, please visit: www.igus.co.uk/smartplastics or call igus directly on: 01604 677240
The terms igus, Apiro, chainflex, CFRIP, conprotect, CTD, drylin, dry-tech, dryspin, easy chain, e-chain, e-chain systems, e-ketten, e-kettensysteme, e-skin, flizz, ibow, igear, iglidur, igubal, kineKIT, manus, motion plastics, pikchain, plastics for longer life, readychain, readycable, ReBeL, speedigus, triflex, robolink, and xiros are protected by trademark laws in the Federal Republic of Germany and internationally, where applicable.All other registered trademarks and trademarks are the property of their respective owners.