12th April, 2020 Simple, precise, fast processes: these are the requirements of Cartesian robots. They are used for such things as pick & place applications, sorting systems and medical technology. igus has now developed a line and room linear robot for large workspaces. The two new kinematics systems allow users to move up to 5kg. […]
7th April, 2020 igus has now added two new sizes to its twisterband HD range with inner heights of 11mm and 18mm. The key advantage over slip ring systems is that it guides electrical, fibre optic and pneumatic cables all together. Target applications include rotary tables and robots. twisterband HD energy chains are already being […]
31st March, 2020 Linear systems are extensively used to move doors, monitors or even panels laterally, or side-to-side. If a low driving force is required, especially for manual adjustments, rollers are often used in the bearing element to reduce friction. However, to absorb the lateral forces, the position of these rollers is crucial. As a […]
17th March, 2020 igus has developed an intelligent bearing that warns of specific wear level, enabling machine and equipment operators to plan maintenance, repairs or part replacement in advance. Called smart iglidur, the intelligent plain bearing was developed for difficult-to-access bearing points and for applications where no regular maintenance intervals have been planned. Defects are […]
10th March, 2020 Robust, lightweight and maintenance-free; these are the key features of the high-performance e-chains from igus. To ensure reliability for users, igus now offers a 36-month guarantee on its e-chains, which matches the similar chainflex cable guarantee. With the online service life calculator, users can now determine the guaranteed runtime of their e-chain […]