New online tool helps users customise the best maintenance-free linear drive system Spindle, rack and pinion, or belt drive? Light or heavy load? Motor or handwheel? The search for the right linear module is time-consuming, which is exactly why igus has introduced the drive technology configurator. After entering all the parameters for the application, this […]
This week’s video shows how igus products are used in vertical farming, an exciting new industry which demands reliability, longevity and no maintenance. This is perfect for igus motion plastics, from smooth gliding drylin® gantries to robust, lightweight e-chains®, the elimination of lubrication means no contamination. To view the video, click here https://youtu.be/lFbmUTzMPXk For more […]
In the machine tool industry, many users worldwide rely on Fanuc motors, drives and controls. In order to supply the drives with fail-safe energy, igus has now developed a new highly flexible servo cable. The cable is specially designed for the dynamic demands when used in energy chains and the cable has an oil-resistant PUR […]
2021 seems to be the year of the drone. In this week’s video you will be introduced to the “drone in the box” system. This allows drones to fly autonomously and automatically, it also serves as a landing platform, control box and offers a station for recharging the battery. In the video, you can see […]
igus develops a blue tribo-filament for cost-effective production of special 3D printed parts for the food industry Responding to customer demand, iglidur I151 is a blue, easy-to-process material and has the best friction and wear values in its class. This new tribo-filament is a further development of the iglidur I150 all-rounder filament from igus. Due […]
In this week’s video of the week, the e-loop® energy chain is shown in extreme temperatures on a drilling rig. The robust energy chain system can withstand the harsh environments of applications such as these while allowing single cables and hoses to be swapped out due to its simple modular design. Protecting the cables is […]
Two new lubrication-free tribo polymers increase the service life of bearings in single-axis solar trackers Solarmid and iglidur P UV are the names of the two new materials that igus has developed specifically for housing bearings in single-axis solar trackers, the panels that track sunlight in solar farms. The new polymers last much longer than […]
A telescopic triflex® TRX energy chain for robots from igus saves space and provides a withdrawal path of up to 40 per cent less. Robots can be limited in their range of movement by the cable retraction system. To allow cables in industrial robots to move safely, easily and compactly, igus has developed the four-dimensional […]
igus launches a new design of a particle-free and lightweight energy guide for clinical environments High abrasion resistance is crucial for machine elements in cleanrooms. In response, igus has developed the C6, an energy chain that is designed to meet the highest cleanroom class. The new chain is specially designed for longer unsupported applications on […]
igus now offers injection moulded, cost-effective production of lubrication-free gears Gears made of polymer deliver power transmission in many applications, from automatic coffee machines to actuators. Specifically for producing wear-resistant and durable gears, igus now offers injection moulded gears in addition to machining from bar stock and those made using additive manufacturing (3D printing). Customers […]