3rd June,2020 As scientists delve into the study of climate change, new strategies and products are evolving to help them uncover data that is driving the world’s foremost crisis. The scientific community is obtaining significant information from international oceans, especially with the support of autonomous surface vehicles. Igus provided data cables and energy chains to […]
20th May, 2020 The CRM rotary module is part of the e-spool flex range and can guide any type of cable or hose, and even corrugated tubes. This compact module has a maximum rotation angle of 6480°, which is 18 full turns, for cable lengths up to 4.5m with a maximum speed of 180°/s and […]
19th May, 2020 In its virtual trade show, igus presents more than 100 plastic innovations and product range additions from all areas of motion plastics. Around 400 square metres in size, the real stand is now open to online visitors and follows the theme ‘Cost down, Life up. It’s our job’. The trade show is […]
8th May, 2020 Curry instead of cola! Five students from Heubach, Germany have developed a vending machine for packaged spices together with engineers and trainees from EMAG LaserTec GmbH. To ensure that the salt, curry and pepper cans are picked from their compartments quickly, they used the drylin W linear guides from igus. Putting academic […]
8th May, 2020 At a time when all the pubs are shut, pouring that perfect pint can prove impossible. igus has solved this problem by providing an easy to use tool for programming its robolink DP robotic arm to ensure it is spot-on every time. With the new Robot Control system, you too can program […]
1st May, 2020 Tech up, Cost down: we will always give you at least one of these. This is our job and for many years has been our promise to you. The immense challenges of this year have spurred us on to even greater efforts. During this uncertain time of change, exhibitions have been cancelled. […]
29th April, 2020 Every day, sensors generate vast amounts of data worldwide and this continues to rise. Single Pair Ethernet (SPE) technology offers completely new opportunities to transmit these data streams reliably even in the most confined areas of the machine. Developed for use in energy chains, igus introduces the chainflex CFBUS.PUR.042 SPE cable. While […]
24th April, 2020 The e-skin energy chain system provides cleanroom equipment with data, power and media without unwanted particles contaminating the air, as proven by the Fraunhofer Institute IPA. All three e-skin energy chain types, with and without cables, have ISO Class 1 certification, which is the ‘cleanest’ classification. In the test conducted by the […]
Whether in handling applications or in laboratory equipment, where there is movement, energy chains are widely used to protect and guide cables and hoses. In the medical industry, however, higher demands are placed on the components, which must all run very smoothly and quietly, be cleanroom-compatible, media-resistant and corrosion-free and of hygienic design. In this […]
15th April, 2020 The challenge for every stage engineer is to create the perfect set, while meeting all related safety and building code standards. In this week’s video, igus shows a range of technologies developed specifically for theatre and stage construction. Here, there are technically challenging requirements, which include high loads, such as those found […]