dry-tech
Whether in handling applications or in laboratory equipment, where there is movement, energy chains are widely used to protect and guide cables and hoses. In the medical industry, however, higher demands are placed on the components, which must all run very smoothly and quietly, be cleanroom-compatible, media-resistant and corrosion-free and of hygienic design. In this […]
12th April, 2020 Simple, precise, fast processes: these are the requirements of Cartesian robots. They are used for such things as pick & place applications, sorting systems and medical technology. igus has now developed a line and room linear robot for large workspaces. The two new kinematics systems allow users to move up to 5kg. […]
31st March, 2020 Linear systems are extensively used to move doors, monitors or even panels laterally, or side-to-side. If a low driving force is required, especially for manual adjustments, rollers are often used in the bearing element to reduce friction. However, to absorb the lateral forces, the position of these rollers is crucial. As a […]
17th March, 2020 igus has developed an intelligent bearing that warns of specific wear level, enabling machine and equipment operators to plan maintenance, repairs or part replacement in advance. Called smart iglidur, the intelligent plain bearing was developed for difficult-to-access bearing points and for applications where no regular maintenance intervals have been planned. Defects are […]
18th February, 2020 Media resistance, lubrication-free and corrosion-free: these are the requirements machine components in the food industry must meet. igus has developed two new materials for its plain and spherical bearings: the iglidur FC180 and igumid FC. Both materials comply with FDA and EU10/2011 regulations and are therefore ideal for use in the food […]
11th February, 2020 Many designers in the industrial sector rely on wear-resistant, high-performance plastic parts for use wherever there is friction between two surfaces. To ensure they get their special plastic part, igus has integrated its Print2Mould process in its online 3D printing service. With a printed tool, the component is manufactured by injection moulding. […]
4th February, 2020 igus has introduced a compact toothed belt axis based on its flat drylin N linear system. The drylin ZLN-40 is 27mm high and 40mm wide and can be delivered with a stroke length of up to 750mm. The modular unit is easy to assemble within minutes or can be ordered and delivered […]
21st November, 2019 Like every competitive athlete, Christopher Young stays acutely attuned to his equipment. Whether it is motorsport, cycling, skiing or any other event where equipment plays an important role in performance, athletes can feel instantly when their equipment is working properly… and when it is not. In Young’s case, however, the margin for […]
17th November, 2019 The use of automated guided vehicles (AGVs) in factories and warehouses is booming. They work around the clock, 7 days a week, 365 days a year. For AGV manufacturers, achieving maximum uptime is a challenge, which can be overcome by using reliable and maintenance-free components. “iglidur tribopolymer bearings, which are used in […]
6th November, 2019 Designing the right shaft for an application is not easy without CAD software and in-depth technical knowledge. igus has now developed a new, free-of-charge and freely accessible online tool with the drylin shaft configurator. In just three steps, designers can select the right shaft in the required length from seven materials, machine […]