e-chain
25th February, 2020 High speeds on long travels are distinct challenges for energy chain systems. To overcome these issues, igus has developed a more wear resistant glide bar, which has a service life that is five times longer. Integrated into the rail is the smart plastics EC.T sensor monitors the condition of the rail and […]
21st January, 2020 To support the circular economy of plastics, igus has invested £4 million in Mura Technology Limited that wants to put the first commercial Catalytic Hydrothermal Reactor (Cat-HTR) plant into operation. The technology recycles plastic waste into oil within 20 minutes, which can be reused to make new plastic products. Every year, 8 […]
10th December, 2019 What happens when a plastic energy chain reaches its maximum service life? Usually, it is disposed of and incinerated with other plastic waste. With its ‘igus green chainge recycling program’, igus is now doing something completely new: users can send their plastic chains to igus for recycling – irrespective of the manufacturer. […]
17th November, 2019 The use of automated guided vehicles (AGVs) in factories and warehouses is booming. They work around the clock, 7 days a week, 365 days a year. For AGV manufacturers, achieving maximum uptime is a challenge, which can be overcome by using reliable and maintenance-free components. “iglidur tribopolymer bearings, which are used in […]
12th November, 2019 igus has introduced the e-loop energy chain for safe cable management on top drives for deep drilling rigs. The new modular system, which is made of high-performance plastic, ensures a defined minimum bend radius of the cables and withstands adverse weather conditions, as well as vibration and shock. In addition to use […]
3rd October, 2019 Guiding power, data and media in confined spaces at high speeds is a major challenge for many OEMs, in particular for intralogistics. With the micro flizz, igus offers a compact energy guidance system for travels up to 100 metres. It consists of an energy chain, flexible chainflex cables suitable for tight bend […]
17th November, 2019 The E2.1 e-chain is the igus standard for small to medium applications. Offering a long service life, quiet operation and easy filling, it is suitable for use in general engineering and machine tool construction. In this week’s video we see how easy it is to open the E2.1 e-chain from the side […]
24th September, 2019 igus has developed its first plastic-steel hybrid energy chain for telescopic applications, such as cherry pickers, telehandlers and boom lifts. Compared to conventional steel energy chains which are sometimes used in these applications, the new YE.42 e-chain is half the weight. It also provides up to 10m unsupported travel, which is 50% […]
September 3rd, 2019 With the e-skin flat and the e-skin soft, igus offers two new space-saving energy chain systems for use in cleanroom applications. Developed for tight installation spaces on short, self-supporting travels, e-skin soft is made of a softer material than the standard e-skin. As the name suggests, e-skin flat is for very flat […]
3rd April, 2020 Although high-performance plastics used to be overlooked as suitable materials for machine components, they are now a standard feature in food processing equipment. But their potential has by no means been exhausted. igus supplies energy chains based on hygienic design guidelines and wear resistant plain bearing components for a wide range of […]