igubal
New generation of igubal spherical plain bearings are equipped with a predictive maintenance system Costly machine failures due to undetected defects in demanding applications should soon be made redundant, thanks to a new generation of two- and four-hole flange bearings with “smart” features. The lubrication-free high-performance plastic bearings are equipped with miniature wireless sensors that […]
Simply switching to a polymer bearing from a stainless-steel bearing has saved a lead acid battery recycler, Fry’s Metals thousands in maintenance costs, and far more in preventing lost production time Recycling lead batteries in high volume is a tough, corrosive working environment to work in. As such, one of South Africa’s leading lead recycling […]
Labour shortages and carbon emissions of petrol mowers means robotic lawn mowers are on the rise. Kingdom Technologies turned to igus to help keep its pay-per-use robotic mower maintenance-free. The greenskeeper surveys drone footage of the golf club. It’s a long fairway and the entire course needs cutting – this one alone could take all […]
The new material iglidur A181 makes the igubal food contact joint system three-times more wear resistant and has several food safety features. To make machines and systems for the food industry even safer, igus has launched the high-performance plastic iglidur A181, a new standard for a spherical ball material for the igubal food contact (FC) […]
The solar industry is growing rapidly and with the help of lubrication-free products, they are changing the way things are produced and how applications operate. In this week’s video of the week, we can see how both igubal® and energy chain parts are used all over the world to help sustainable applications. To view the […]
igubal stainless steel rod ends with iglidur A160 enable lubrication-free dry running with no risk of contamination Constant relubrication of metal bearing points in the food industry costs time, money and increases the risk of contamination. Maintenance-free igubal spherical plain bearings from igus are an economical and safe alternative. Now igus has introduced a new […]
New igubal bearings are a maintenance-free, economical alternative to classic cast housing bearings. Nature can provide engineering with great inspiration: The shape of the new igubal pillow block bearings is based on the design of a tree. Flattened radii ensure maximum strength against mechanical stresses, like a tree’s base. Thanks to this bionic shape, these […]
Grease is a thing of the past! It’s the dirty and costly way of lubricating your bearings and moving parts. In the future it will be outed as the combustion engine of the mechanical work and users will be searching for that new and efficient way of keeping production lines and other equipment running. You […]
In this week’s video of the week, it is obvious of the main benefit of changing your metal bearings for igus® polymer ones. The various igubal® parts shown start covered in grease but by switching to a lubrication free igus® bearing, this is eradicated. To watch the video, click here https://youtu.be/TJD0QPeqLzE For more information on […]
A new elastic double joint from plastics specialist igus is proving to be a perfect – and quiet – solution for the machine building sector. The igubal GPZM coupling joint, which was officially launched at the end of 2020, is lubrication-free, maintenance-free and 20% more flexible than its conventional alternative. Dean Aylott, Product Manager at […]