Machine tools

There are a total of 51 files available
The MH HEIDI device can equip two machine tools at the same time
File type: image, JPEG

The KMC-G machining centre is designed for workpieces from the aerospace and machinetool industries.
File type: image, JPEG

The machining centre is equipped with an exchange device for the milling spindle.
File type: image, JPEG

The X-axis travel distance of the KMC-G is over 13 meters.
File type: image, JPEG

Path length and the number of cables require a special e-chain
File type: image, JPEG

pivoting roll holders allow free movement of the chain and support the upper run
File type: image, JPEG

preassembled readychains shorten the installation time of cables considerably
File type: video, MPEG4

The e-chains are delivered as preassembled readychains including mounting frame.
File type: image, JPEG

Energy chains ensure reliable energy supply in gantry processing systems
File type: image, JPEG

The assembly of this chain took only a few hours instead of days as with conventional cables.
File type: image, JPEG

the chainflex cables in the e-chain also come from igus
File type: image, JPEG

Assembly of a MultiTHerm system in Brazil, including igus e-chains
File type: image, JPEG

Messer's current showcase project is the MultiTherm system with igus e-chains
File type: image, JPEG

For Z-axis applications, the closed version of the energy chain is used.
File type: image, JPEG

The L-version of the Energy Chain E4.1 is particularly stable
File type: image, JPEG

Due to the locking mechanism, the energy chain can be equipped very quickly
File type: image, JPEG

Energy chains on X- and Y-axis of the linear robot
File type: image, JPEG

A press removal device removes cutting plates from the press and palletizes them for the subsequent sintering process
File type: image, JPEG

Information about the downloads:
On this page you get access to media material which is protected by copyright. The material may only be used for reporting purposes, including print media, online media, blogs, forums, social media channels, radio and television.

The material may only be used if the source "igus GmbH" is cited. Any other usage, whether for commercial or purely private purposes, is not permitted.

If you do not find pictures, videos or texts in the download area, you can also send an image request to pressoffice-internationalde@igus.net.