drylin
2021 seems to be the year of the drone. In this week’s video you will be introduced to the “drone in the box” system. This allows drones to fly autonomously and automatically, it also serves as a landing platform, control box and offers a station for recharging the battery. In the video, you can see […]
In this week’s video of the week, It is all about drylin®! To celebrate the new drylin® product information webpages, this week’s video highlights all the key benefits of using drylin® over alternatives. The lightweight, dirt resistant, sustainable linear systems sell themselves. To view the video, click here https://youtu.be/qOOYXw0Z1DY For more information on the drylin® […]
New bearings made of iglidur W360 high-performance plastic ensure precise and easy linear movements The new iglidur W360CM series linear bearings are designed to slide on round shafts with high precision. The linear bearing consists of an aluminium housing and a polymer liner, which ensures high accuracy. The design allows precise movement. By using iglidur […]
The manus award- igus’s awards programme for polymer bearing applications, received 582 entries in 2021. Back in 2019, The iFLY15 catamaran won silver in the manus awards and is now attempting to break a world record. Twin-hulled catamarans are designed to lift out of the water on hydrofoils, and the iFLY15 sports catamaran from CEC […]
With the new igus® ReBel cobot, it is now even easier to accomplish robot/human collaborative tasks. These robots are suitable for assembly aids, pick & place tasks and can be used within industrial or private applications. See how smooth it moves in this week’s video of the week: https://youtu.be/BNjg5HaoWio For more information on the igus® […]
This week’s video of the week shows how a range of igus® products are utilised in a production of disposable face masks. Unfortunately, facemasks have become a staple in our lives. So much so, manufacturers have now recognised the benefits of igus® products within this manufacturing sector. Clean, dry and lubrication free means that all […]
The igus® drylin® range is known for being lubrication-free, robust and will never shy away from a challenge! In this week’s video of the week, the drylin® telescopic rails are put to the test being covered in dirt, sand and water. See how well they cope in such environments. To view the video, click here […]
Telescopic slides are used within all kinds of applications, from kitchens, furniture to aircraft and automotive. This new NTP-27 all polymer telescopic slide is manufactured using igus®‘ iglidur® materials giving all the benefits of our dry running maintenance free and lubrication free dynamics whilst having the added aesthetic feature of many different colour options to […]
igus® robolink® DP can now be used in splash water applications with a protection class of IP44. In this week’s video of the week you will see how not only the robolink® robot arm copes with water but also an igus® colleague. To watch the video please visit https://youtu.be/9glNMERKzsQ For more information regarding the Robolink® range please visit https://www.igus.co.uk/info/robotics-robolink or call igus® directly on: 01604 […]
A ready-to-fit 7th axis has been designed and manufactured by igus to enable Universal Robots (UR) and robolink robots to travel several metres. The global manufacturer of energy chain systems and polymer plain bearings,which has its UK headquarters in Northampton, has developed this robotic solution to include amaintenance-free, drylin ZLW toothed belt axis, corresponding adapter […]