drylin
29th July, 2020 A drylin W linear guide fitted with a PRT slewing ring bearing provides linear and rotating motion. This new design study from igus can move linearly and rotate simultaneously. With the drylin W linear/pivot guide, armrests, trays and control panels on seats and armchairs, for example, can be easily adjusted to suit […]
30th June, 2020 igus has developed control software for its low-cost automation solutions that allows users to easily program their robots. Available online, free of charge, the igus robot control software enables different robot kinematics to be programmed and controlled. A digital twin simulates the movements, allowing the user to program a suitable solution before […]
26th June, 2020 The innovative Camping Butler cleans mobile toilet cartridges, from caravans and camper vans, fully automatically and contact-free from the inside and outside. No matter how full or very dirty the cassette is, the Camping Butler cleans it completely. In the week’s video, we go behind the scenes to see how exactly the […]
19th May, 2020 In its virtual trade show, igus presents more than 100 plastic innovations and product range additions from all areas of motion plastics. Around 400 square metres in size, the real stand is now open to online visitors and follows the theme ‘Cost down, Life up. It’s our job’. The trade show is […]
8th May, 2020 Curry instead of cola! Five students from Heubach, Germany have developed a vending machine for packaged spices together with engineers and trainees from EMAG LaserTec GmbH. To ensure that the salt, curry and pepper cans are picked from their compartments quickly, they used the drylin W linear guides from igus. Putting academic […]
8th May, 2020 At a time when all the pubs are shut, pouring that perfect pint can prove impossible. igus has solved this problem by providing an easy to use tool for programming its robolink DP robotic arm to ensure it is spot-on every time. With the new Robot Control system, you too can program […]
1st May, 2020 Tech up, Cost down: we will always give you at least one of these. This is our job and for many years has been our promise to you. The immense challenges of this year have spurred us on to even greater efforts. During this uncertain time of change, exhibitions have been cancelled. […]
12th April, 2020 Simple, precise, fast processes: these are the requirements of Cartesian robots. They are used for such things as pick & place applications, sorting systems and medical technology. igus has now developed a line and room linear robot for large workspaces. The two new kinematics systems allow users to move up to 5kg. […]
31st March, 2020 Linear systems are extensively used to move doors, monitors or even panels laterally, or side-to-side. If a low driving force is required, especially for manual adjustments, rollers are often used in the bearing element to reduce friction. However, to absorb the lateral forces, the position of these rollers is crucial. As a […]
4th February, 2020 igus has introduced a compact toothed belt axis based on its flat drylin N linear system. The drylin ZLN-40 is 27mm high and 40mm wide and can be delivered with a stroke length of up to 750mm. The modular unit is easy to assemble within minutes or can be ordered and delivered […]