Keyword:

energy chains

Customer consultations and R&D leave igus well-prepared for PFAS ban 

Published on: 27/08/2024

The plastics industry is preparing for a potential ban of fluoropolymers, or PFAS, a group of versatile polymers that have many industrial applications. igus® has increased R&D resources for developing viable non-PFAS solutions, and is working with customers in automotive, medical, packaging and other industries, to find fully tested alternative materials if required.  Motion plastics […]

Read more...

The Tung Auditorium: igus® HD e-spool® supports award-winning Concert Hall

Published on: 25/06/2024

The Tung Auditorium in the heart of the University of Liverpool’s campus has undergone an incredible transformation, with the help of igus®, to enhance both the acoustic technology and architectural design, resulting in the venue winning at the MONDO-DR Awards in the concert hall category. Situated within the Yoko Ono Lennon Centre, The Tung Auditorium […]

Read more...

Smooth entertainment aboard, even in rough seas thanks to igus and Videlio-HMS

Published on: 17/06/2024

At French shipyard Chantiers de l’Atlantique, theatres and entertainment systems supplied by Videlio-HMS must pass rigorous standards to run smoothly at sea. Cables and energy supply systems supplied by igus are chosen for their reliability and maritime standards. Life at sea is very different to life on dry land; ask any seafarer. And all the […]

Read more...

New igus compact low-cost energy chain designed for drawers

Published on: 02/05/2024

Through downsizing, the draw-e-chain saves 30% in costs in applications with occasional movement igus has launched the draw-e-chain for cable routing in drawers and pull-out  applications like server racks. Thanks to its minimal structural design, this compact energy chain costs 30% less than that of the most cost-effective standard e-chains. This prevents costly oversizing, especially […]

Read more...

Ready-to-install energy chains fitted more easily, quickly and precisely

Published on: 31/01/2024

Save installation time and improve handling: igus’s popular readychain service is complete with a new “assembly helper” device: the “fastpositioner” Idle machines and systems cost manufacturing companies valuable time and money. To make it easier for customers to install energy supply systems and reduce installation time, igus’s readychain service offers pre-assembled cable systems consisting of […]

Read more...

snapchain 2.0: Compact, low carbon, and cost-effective energy management

Published on: 14/11/2023

New igus energy chain can be installed in seconds and is the second igus e-chain series to be made of 100% recycled material. The simplest products are often both the most cost-effective, and the best technically. igus has now developed snapchain 2.0, a sustainable energy chain especially for simple, flat cable packages made of 100% […]

Read more...

igusGO: AI-driven, cost-saving machine design optimisation app makes work fun

Published on: 07/11/2023

By harnessing AI, a new igus app shows how to optimise the design of over 450 applications in just a few seconds Wouldn’t it be nice if time-poor engineers, faced with huge component choices, could easily and quickly improve their designs by seeing the full range of components and their properties instantly? Step forward the […]

Read more...

Wanted: Unique applications for energy chain systems, igus vector awards

Published on: 31/10/2023

Win up to 5,000 euros as the ninth “vector award” for different and sustainable e-chain solutions opens for applications. Deadline: February 9, 2024 Attention all machinery engineers: The vector award from igus has entered the next round. For the ninth time, the award recognises designers and project managers who show creativity and imagination in the […]

Read more...

New particle-free energy chain from igus for SCARA robots in cleanrooms

Published on: 21/09/2023

Clean SCARA Cable Solution works almost particle-free to ISO class 2 igus has launched a new energy supply system for SCARA robots in cleanrooms: the Clean SCARA Cable Solution consists of tribologically optimized high-performance plastics and works in almost particle-free conditions specified to ISO class 2 even in high-speed applications. The system is also highly […]

Read more...

Highest safety in battery production: first energy chain to be certified for dry cleanrooms

Published on: 01/08/2023

Test passes with flying colours: igus’ E6.29 energy chain receives innovative dry cleanroom certificate from research consultancy Fraunhofer IPA for ISO Class 4 Whenever the highest hygiene standards are required, igus scores well with lubrication-free and abrasion-resistant motion plastic components. A topical example is that battery production for electric vehicles requires special environmental conditions, which are […]

Read more...