heavy duty
igus launches a new lubrication-free material, for bearings needing higher running performance with high dynamic forces, ideal for heavy-duty applications. igus has developed plain bearings made from high-strength, fibre-wound materials – the igutex bearing family. These use carbon fibre embedded in the material and are used where very high impact loads occur and where injection-moulded […]
iglidur Q3E plain bearings, now manufactured by injection moulding, ensure lubrication-free maximum load capacity performance, made using efficient high-volume production An important industry first for the construction and agricultural machinery industries: For the first time igus has found a way to manufacture heavy-duty bearings made from two components of high-performance plastic, using the cost-effective injection […]
igus launches a new lubrication-free material, for bearings needing higher running performance with high dynamic forces, ideal for heavy-duty applications. In applications with loads of more than 80Mpa, plain bearings made of thermoplastic materials can be pushing their physical limits. Igus has expanded the existing range of standard plain bearings with the new igutex fibre-wound […]
igus develops P4HD roller e-chain with wear-resistant materials, and smart monitoring. Next generation cranes need higher power supplies. Energy chains – the protective chains that transport power and control cables in linear motion – must meet these requirements for longer travels, higher accelerations and operational uncertainties, as well as high reliability. The new igus heavy-duty […]
6th August, 2020 Brickworks are very harsh environments for any product, from the extreme dust and aggressive dirt to the high loads and fluctuating temperatures. igus® energy chains protect the encapsulated cables whilst continuing to meet the high demands of the application. These chains endure severe conditions but thanks to their reinforced configuration this has […]