Keyword:

iglidur

VOTW- Freedom of design with stock material

Published on: 11/11/2021

Sometimes having a nonstandard part can be problematic and expensive. Thankfully with the igus® stock material range, this doesn’t need to be the case. With a large variety of materials, with different temperature ranges and different mechanical properties, the iglidur® stock materials are suitable for a multitude of applications. In this week’s video of the […]

Read more...

Maintenance-free knife edge rollers expand the igus online shop range

Published on: 21/09/2021

iglidur rollers with predictable service life ensure product transport in food technology So that users can get their wear-resistant knife edge roller even faster, igus has expanded its online shop to include the range of iglidur rollers made from high-performance polymers. Included in the new range are knife edge rollers made of the blue material […]

Read more...

Safe sorting even in heat: New igus material for the food industry

Published on: 15/09/2021

Electrostatically dissipating iglidur AX500 tribopolymer ensures maintenance-free, food industry applications In the food and packaging industry, sorting and packing zones are subject to constant movement of goods and temperature changes. For these storage mechanisms to perform flawlessly, long-lasting plain bearing solutions are required that can withstand friction and heat long-term. Another challenge is the creation of […]

Read more...

Sustainability at the push of a button: e-chain for Drop Water vending machine

Published on: 07/09/2021

A new water vending machine from a Californian company reduces the transport and consumption of plastic bottles with the help of igus motion plastics. The Drop Station is a new sustainable drinks vending machine that dispenses water into compostable containers at the push of a button. The water does not have to be transported, as […]

Read more...

iglidur I151 for safe, FDA-compliant and detectable consumable parts in food technology

Published on: 19/08/2021

igus develops a blue tribo-filament for cost-effective production of special 3D printed parts for the food industry Responding to customer demand, iglidur I151 is a blue, easy-to-process material and has the best friction and wear values in its class. This new tribo-filament is a further development of the iglidur I150 all-rounder filament from igus. Due […]

Read more...

High factor protection: igus develops solar materials with three-times more UV-resistance

Published on: 06/08/2021

Two new lubrication-free tribo polymers increase the service life of bearings in single-axis solar trackers Solarmid and iglidur P UV are the names of the two new materials that igus has developed specifically for housing bearings in single-axis solar trackers, the panels that track sunlight in solar farms. The new polymers last much longer than […]

Read more...

Wear-resistant polymer gears from igus: Printed, machined and now injection moulded

Published on: 20/07/2021

igus now offers injection moulded, cost-effective production of lubrication-free gears Gears made of polymer deliver power transmission in many applications, from automatic coffee machines to actuators. Specifically for producing wear-resistant and durable gears, igus now offers injection moulded gears in addition to machining from bar stock and those made using additive manufacturing (3D printing). Customers […]

Read more...

Maximum precision: new drylin linear bearings for round shafts

Published on: 06/07/2021

New bearings made of iglidur W360 high-performance plastic ensure precise and easy linear movements The new iglidur W360CM series linear bearings are designed to slide on round shafts with high precision. The linear bearing consists of an aluminium housing and a polymer liner, which ensures high accuracy. The design allows precise movement. By using iglidur […]

Read more...

Compact rotation: igus expands range of slewing rings for tight spaces

Published on: 29/06/2021

The space-saving PRT-04 slewing ring bearings are now available in a range of sizes with inner and outer tooth drives and a locking function. Compact and lightweight, the new bearings have been developed specifically for movement in tight spaces and give igus an entire PRT-04 modular system. The lubrication-free, slewing ring bearing system comes in […]

Read more...

The circular economy and igus give plastics a second life

Published on: 10/06/2021

Environmental protection is gaining more momentum today and plastic is a big part of this. Social transformation, responsibility for sustainability and the changes in our use of plastics are not going unnoticed by industry. Examples from igus, the motion plastics specialist, show how companies can use engineering and ecological innovations to tackle these issues. More […]

Read more...