igus bearings
As well as increasing the number of low carbon and renewable products and services in 2023, igus uses a reliable carbon tracking method for suppliers and can now provide the carbon content of most iglidur products. It aims to show the carbon content of all its products by mid-2024. Companies are under growing pressure to […]
igus launches a new lubrication-free material, for bearings needing higher running performance with high dynamic forces, ideal for heavy-duty applications. In applications with loads of more than 80Mpa, plain bearings made of thermoplastic materials can be pushing their physical limits. Igus has expanded the existing range of standard plain bearings with the new igutex fibre-wound […]
Labour shortages and carbon emissions of petrol mowers means robotic lawn mowers are on the rise. Kingdom Technologies turned to igus to help keep its pay-per-use robotic mower maintenance-free. The greenskeeper surveys drone footage of the golf club. It’s a long fairway and the entire course needs cutting – this one alone could take all […]