plain bearings
Lubrication-free and maintenance-free high-load material iglidur TX2 demonstrates 3.5-fold improved wear performance in tests. Especially forhigh-load applications in the construction, machinery, or agricultural industries, igus can now offer the new Tribo (tribologically optimized) material iglidur TX2, which works without lubrication. Even smaller excavating machines still need about 50 litres of lubricant per year with metal […]
igus experts present how motion plastics can reduce costs and sustainably improve technology in a series of live shows Our mobility is changing rapidly: e-scooters, e-bikes, e-cars and vehicles with alternative power sources are increasingly common. The concept of car sharing is also establishing itself in cities worldwide. At the IAA Mobility Show 2021 in […]
New i.Cee:local module predicts the service life of machines and manufacturing systems, making maintenance more efficient and predictable Motion plastics leader igus has developed a new predictive maintenance device, a new home for the software to power its smart plastics products – the i.Cee:local module. The module calculates the remaining service life of the energy […]
The manus award- igus’s awards programme for polymer bearing applications, received 582 entries in 2021. Back in 2019, The iFLY15 catamaran won silver in the manus awards and is now attempting to break a world record. Twin-hulled catamarans are designed to lift out of the water on hydrofoils, and the iFLY15 sports catamaran from CEC […]
The new robolink IP44 from igus: a robot that defies water! Requests by customers for a robolink fit for wet conditions has prompted plastics expert igus to design one that can withstand rain, showers, and moisture. The company, which has its UK headquarters in Northampton, has developed its very first water-resistant robolink – a low-cost […]
17th November, 2019 The use of automated guided vehicles (AGVs) in factories and warehouses is booming. They work around the clock, 7 days a week, 365 days a year. For AGV manufacturers, achieving maximum uptime is a challenge, which can be overcome by using reliable and maintenance-free components. “iglidur tribopolymer bearings, which are used in […]
24th September, 2019 For air conditioning systems in buildings, aircraft and cars, mould is not only a great annoyance but a serious health hazard. To prevent this, mould-resistant components must be used. Therefore, igus had its materials tested for mould growth. The result: seven igus plain bearing materials are resistant to fungi and bacteria. In […]