slewing ring
The new lubrication-free iglidur slewing ring bearing PRT-04 Micro for very small installation spaces is the latest in a high-performing product series. Miniaturisation means requirements for machine components are becoming increasingly demanding, where enabling movement in the smallest installation spaces is an engineering challenge for many companies. Now igus has further developed its PRT-04 slewing […]
Never has a video highlighted the versatility of igus® products so well. When you think of a train you think industrial, massive loads and extremely dirty but using igus® products can eliminate some of those preconceptions. No grease required, durable so capable of high loads and made from hard wearing plastic! In this week’s video […]
Have you ever considered all the applications where things turn? There are thousands!! And to help these applications turn with a smooth motion, customers are using the igus® PRT slewing ring bearing. These bearings are low-cost, maintenance free and require no lubrication! In this weeks’ video of the week, the PRT shows the ease to […]
New locking function of iglidur PRT slewing ring bearings removes need for time-consuming adjustments With a new locking mechanism, igus adds more functions to its lubrication- and maintenance-free slewing ring bearings in the PRT-04 series for tight installation spaces. This saves time in adjusting, for example, assembly tables, jigs, fixtures and control panels. Fitters and […]
The space-saving PRT-04 slewing ring bearings are now available in a range of sizes with inner and outer tooth drives and a locking function. Compact and lightweight, the new bearings have been developed specifically for movement in tight spaces and give igus an entire PRT-04 modular system. The lubrication-free, slewing ring bearing system comes in […]
Whether in handling applications or in laboratory equipment, where there is movement, energy chains are widely used to protect and guide cables and hoses. In the medical industry, however, higher demands are placed on the components, which must all run very smoothly and quietly, be cleanroom-compatible, media-resistant and corrosion-free and of hygienic design. In this […]