chainflex
Long service life of igus chainflex high-end TPE cables convinces inspectors and gives customers certified safety igus is the first cable manufacturer in the world to receive UL AWM certification from US validation agency Underwriters Laboratories (UL) for its high-end TPE cables, which do not require fire-retardant halogens as additives. This is the first time […]
igus has introduced ready-made cables for the Single Pair Ethernetespecially for e-chain use Single Pair Ethernet (SPE), which uses a single twisted pair of conductors that reduces the cable thickness and the size of the connectors required, is now one of the biggest trends in data communication for devices to communicate with the smallest sensors. […]
A new water vending machine from a Californian company reduces the transport and consumption of plastic bottles with the help of igus motion plastics. The Drop Station is a new sustainable drinks vending machine that dispenses water into compostable containers at the push of a button. The water does not have to be transported, as […]
In the machine tool industry, many users worldwide rely on Fanuc motors, drives and controls. In order to supply the drives with fail-safe energy, igus has now developed a new highly flexible servo cable. The cable is specially designed for the dynamic demands when used in energy chains and the cable has an oil-resistant PUR […]
New flexible chainflex Profinet cable saves time-consuming assembly with knife and pliers igus now offers a new chainflex Profinet cable for the fast connection of cables in the field. For this purpose, igus has developed “FastConnect” technology, allowing the cable to be easily stripped in just a few simple steps, reducing assembly time by 46 […]
A new chainflex cable box is proving a best seller for plastics expert igus. The chainflex CASE, a new logistics solution from this global manufacturer of energy chain systems and polymer plain bearings, is saving customers both time and money. John Barker, chainflex cable product manager at igus, which has its UK headquarters in Northampton, […]
igus® has developed the e-rib to safely guide cables inside corrugated hoses. Now it has developed a system of reinforcements at both ends as well as rotary unions, to offer a full solution for high-speed SCARA applications.The system is easy to retrofit or can be delivered as a fully harnessed system with igus® chainflex® cables. […]
igus has joined the world’s largest automation membership body to advance the research of Profinet technology in dynamic applications. The focus for PROFIBUS & PROFINET International (PI), which has more than 1,700 members worldwide, is the continuous development of Profibus and Profinet technology, the two most important enabling technologies in automation today. igus, which has […]
12th August, 2020 Side-mounted energy chain from igus ensures reliable energy supply in high-speed lightweight linear robots Twice as fast at half the weight: this is what makes the linear motor robot from FIBRO LÄPPLE TECHNOLOGY (FLT) different from many other solutions. In order for the linear robot to be able to get production up […]
6th August, 2020 In order to supply modern motors with energy and data, users need appropriate cables that function reliably, even at high accelerations and on long travels. Especially for dynamic use, igus has now developed a hybrid cable that is offered as a drive solution for the new Bosch Rexroth motors. It combines an […]