e-chain
3rd June,2020 As scientists delve into the study of climate change, new strategies and products are evolving to help them uncover data that is driving the world’s foremost crisis. The scientific community is obtaining significant information from international oceans, especially with the support of autonomous surface vehicles. Igus provided data cables and energy chains to […]
20th May, 2020 The CRM rotary module is part of the e-spool flex range and can guide any type of cable or hose, and even corrugated tubes. This compact module has a maximum rotation angle of 6480°, which is 18 full turns, for cable lengths up to 4.5m with a maximum speed of 180°/s and […]
19th May, 2020 In its virtual trade show, igus presents more than 100 plastic innovations and product range additions from all areas of motion plastics. Around 400 square metres in size, the real stand is now open to online visitors and follows the theme ‘Cost down, Life up. It’s our job’. The trade show is […]
1st May, 2020 Tech up, Cost down: we will always give you at least one of these. This is our job and for many years has been our promise to you. The immense challenges of this year have spurred us on to even greater efforts. During this uncertain time of change, exhibitions have been cancelled. […]
24th April, 2020 The e-skin energy chain system provides cleanroom equipment with data, power and media without unwanted particles contaminating the air, as proven by the Fraunhofer Institute IPA. All three e-skin energy chain types, with and without cables, have ISO Class 1 certification, which is the ‘cleanest’ classification. In the test conducted by the […]
Whether in handling applications or in laboratory equipment, where there is movement, energy chains are widely used to protect and guide cables and hoses. In the medical industry, however, higher demands are placed on the components, which must all run very smoothly and quietly, be cleanroom-compatible, media-resistant and corrosion-free and of hygienic design. In this […]
15th April, 2020 The challenge for every stage engineer is to create the perfect set, while meeting all related safety and building code standards. In this week’s video, igus shows a range of technologies developed specifically for theatre and stage construction. Here, there are technically challenging requirements, which include high loads, such as those found […]
12th April, 2020 Simple, precise, fast processes: these are the requirements of Cartesian robots. They are used for such things as pick & place applications, sorting systems and medical technology. igus has now developed a line and room linear robot for large workspaces. The two new kinematics systems allow users to move up to 5kg. […]
7th April, 2020 igus has now added two new sizes to its twisterband HD range with inner heights of 11mm and 18mm. The key advantage over slip ring systems is that it guides electrical, fibre optic and pneumatic cables all together. Target applications include rotary tables and robots. twisterband HD energy chains are already being […]
10th March, 2020 Robust, lightweight and maintenance-free; these are the key features of the high-performance e-chains from igus. To ensure reliability for users, igus now offers a 36-month guarantee on its e-chains, which matches the similar chainflex cable guarantee. With the online service life calculator, users can now determine the guaranteed runtime of their e-chain […]